+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Semiconductor is a material with electrical properties intermediate between a conductor and an insulator, characterized by the ability to control the conduction of electricity depending on external conditions such as temperature, electric field, light, or doping. Its crystalline structure allows the presence of a conduction band and a valence band separated by an energy gap, the width of which determines how easily electrons can move to energy levels capable of conducting electricity.
In its pure state, semiconductors such as silicon or germanium conduct very little current, but their conductivity can be significantly increased by introducing small amounts of foreign atoms—a process called doping. Depending on the type of dopant used, n-type semiconductors are created, where charge carriers are electrons, and p-type semiconductors, where conduction occurs through holes, or electron vacancies in the crystal structure. A p-n junction, formed at the interface of these two areas, is the basis for the operation of many electronic components, including diodes, transistors, and integrated circuits.
The ability to precisely control conductivity properties makes semiconductors the foundation of modern electronics. Their behavior is described using solid-state physics and band theory, which enables the design of structures with specific logical, amplifying, switching, or light-emitting functions. Depending on the manufacturing technology, various epitaxial, lithographic, and chemical techniques are used to form microstructures at the nanometer scale.
Semiconductors are used not only in consumer and industrial electronics but also in optoelectronic systems, photovoltaics, sensors, wireless communication, and quantum technologies. Their properties can also be modified by exposure to radiation, pressure, or magnetic fields, making them extremely versatile materials in scientific and technological applications.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.