+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Electric charge is a fundamental physical property of matter that determines its ability to interact via electrostatic and electromagnetic forces. It is one of the basic concepts in classical and quantum physics, serving as the source of the electric field and defining the strength of interactions between particles. In the SI system, electric charge is measured in coulombs (C), with the smallest indivisible unit being the elementary charge carried by particles such as the electron (negative charge) and the proton (positive charge).
In nature, charges exist in two forms: positive and negative. Bodies with opposite charges attract each other, while those with like charges repel. These phenomena are described by Coulomb’s law, which is the foundation for analyzing electrostatic forces between objects. Electric charge is a conserved quantity, meaning that the total charge in a closed system remains constant regardless of physical or chemical transformations.
At the microscopic level, charge mediates electromagnetic interactions and participates in processes such as conduction, ionization, and recombination. In electrical conductors like metals, free charges (typically electrons) can move under the influence of an electric field, resulting in electric current. In insulators, charge movement is highly restricted, allowing them to be used for isolating circuits and preventing uncontrolled current flow.
Phenomena associated with electric charge play a key role in the operation of electronic systems, measuring devices, power systems, and signal processing technologies. The presence and distribution of charge influence the electric field and electric potential, and in the context of electromagnetic dynamics, also contribute to the generation of magnetic fields. In quantum physics, charge is also a defining characteristic of elementary particles, affecting their behavior in external fields and interactions with other particles.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.