+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Programmers and debuggers from Segger at TME

Date of publication: 24-01-2024 🕒 1 min read

Segger is a German manufacturer of products for embedded systems. The company was established in the 1990s and nowadays it has offices in e.g. Shanghai, the UK and the USA. Thanks to this, Segger is able to provide the best service and support to customers around the world. What is more, a significant advantage of the solutions offered by Segger is their compatibility with the most popular development environments and operating systems (Linux, macOS and Windows), which facilitates their implementation and use.

In the TME catalogue, you can now find programmers and debuggers that are compliant with the JTAG standard, which are suitable for ARM7/9/11- or Cortex A/M/R-based circuits and products from the PIC32, RISC-V, EFM8 and RENESAS RX series. It is also worth taking a look at the J-Link debuggers, which exhibit high communication speed with supported microcontrollers and high Flash programming speed reaching up to 1 MB/s, provide an unlimited number of breakpoints set during debugging, and support every popular architecture (ARM, RISC-V, Microchip, Renesas RX, SiLabs 8051, Cadence Tensilica).

Check out the Segger products available at TME

Download
If you would like to use the article, please cite TME as the source and add a link to the original text when republishing it online.

rightColumnPicture rightColumnPicture

READ ALSO