+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
ASCII (American Standard Code for Information Interchange) is a widely adopted character encoding standard developed in the United States during the 1960s to standardize the representation of textual data in digital systems. It is based on a 7-bit binary code, allowing for the encoding of 128 characters, including Latin alphabet letters, digits, punctuation marks, symbols, and control characters.
The ASCII standard enables communication between electronic devices—such as computers, terminals, printers, and modems—by assigning each character a unique numerical value. This uniform encoding allows text to be stored, transmitted, and interpreted consistently, regardless of hardware or operating system. The original ASCII version includes only characters used in English, which limits its applicability for other national languages.
To address these limitations, several ASCII extensions were developed, including 8-bit encodings (e.g., ISO 8859-1) and later multibyte standards such as Unicode, which allow representation of characters from various languages and scripts. Nevertheless, ASCII remains the foundation of modern text encoding systems and continues to be widely used in device communication, network protocols, text files, and programming—where it frequently serves as the basis for defining characters and performing string operations.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.