+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Curie temperature - definition

Curie temperature is the characteristic temperature value above which ferromagnetic materials lose their magnetic properties and change to a paramagnetic state. This phenomenon is due to the breakdown of the ordered arrangement of the magnetic moments of the atoms, which at temperatures below Curie allows spontaneous magnetisation of the material. Beyond this limit, the thermal vibrational energy of the atoms becomes large enough to interfere with the spin interactions, leading to the decay of the ordered arrangement of magnetic domains.

The Curie temperature depends on the type of material and its crystal structure, and its value is constant for a given substance. For iron it is about 770°C, for nickel 358°C and for cobalt 1130°C. This phenomenon also applies to ferrite and piezoelectric materials, where the Curie temperature determines the limit of the phase transition, important for their functional properties such as magnetic susceptibility or the ability to generate an electrical charge under mechanical deformation.

In the case of dielectrics ferroelectrics, the Curie temperature determines the moment of transition from the ferroelectric to the paraelectric phase, which affects changes in relative electrical permeability and spontaneous polarisation. This phenomenon is widely used in technologies related to sensors, resonators, Ceramic capacitors and shape memory materials. The measurement and control of Curie temperature is important in the design of electronic and magnetic devices, especially where the stability of material properties is critical to system performance.

The concept of Curie temperature is named after Pierre Curie, who conducted pioneering research into the magnetic properties of solids and was the first to describe thermal magnetic transition phenomena.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO