+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Ohm's Law

The Ohm's law calculator allows for quick calculation of the relationship between voltage (V), current intensity (A), resistance (Ω), and power (W). Just enter at least two known values, and the tool will automatically calculate the remaining parameters based on Ohm's law formulas and power relationships. It is a practical aid in designing, diagnosing, and analyzing electrical and electronic circuits.

What is the Ohm's Law calculator used for?

The Ohm's Law calculator simplifies calculations that appear literally at every step in electronics. It allows you to quickly check:

  • what current will flow through an element with a known resistance at a given voltage,
  • what resistance a resistor should have to limit the current to a safe value,
  • what power will be dissipated by a resistor, heater or other load.

This allows you to preliminarily select the values of elements at the design stage, assess the load on the power supply or wires, and also verify whether the existing system is not operating outside the safe range of parameters.

Basic quantities: V, I, R, P

To comfortably use the calculator, it is worth reminding yourself what the individual symbols mean.

Voltage (V)

Electric voltage is the potential difference between two points in the circuit. In practice, it determines the "force" with which the power source "pushes" electrons in the conductor. Typical values encountered in electronics include:

  • 3.3V and 5V - power supply of microcontrollers and digital logic,
  • 12V - automotive systems, LED lighting, fans,
  • 24V - industrial automation,
  • 230V AC - power grid in home installations (safety is particularly important here).

In the calculator, we enter the voltage in volts (V).

Current intensity (I)

The current intensity describes how much charge flows through the cross-section of the conductor per unit of time. In practice, it determines:

  • power supply load,
  • heating of wires and elements,
  • selection of fuses and protections.

We express current in amperes (A), although in small electronic systems we often operate in milliamperes (mA). The calculator accepts values in amperes and on this basis calculates the remaining quantities.

Resistance (R)

Resistance is the electrical resistance that "inhibits" the flow of current. Every circuit element - resistor, wire, PCB track, connector - has some resistance, although for many of them it is very small. We measure resistance in ohms (Ω).

Choosing the right resistance allows:

  • to limit the current (e.g. in LED diodes),
  • to set voltage dividers,
  • to shape the characteristics of filters and RC circuits.

Power (P)

Electrical power determines how quickly energy is converted into another form - e.g. heat or light. We measure it in watts (W). In practice, power informs how much the element heats up and what power supply is needed.

Knowledge of power is crucial when:

  • selecting resistors with the appropriate nominal power (¼W, 0.5W, 1W, etc.),
  • assessing the heating of transistors, stabilizers or heaters,
  • planning the energy balance of the entire device.

How the Ohm's Law calculator works - discussion of formulas

The Ohm's Law calculator is based on several basic relationships that connect voltage, current, resistance and power.

Basic Ohm's Law formulas:

  • V = I × R - voltage is equal to current multiplied by resistance,
  • I = V / R - current is voltage divided by resistance,
  • R = V / I - resistance is voltage divided by current.

Relationships for power:

  • P = V × I - power is the product of voltage and current,
  • P = I² × R - the power dissipated on the resistor can be calculated from the current and resistance,
  • P = V² / R - or from voltage and resistance.

Using the calculator is simple:

  1. Enter at least two known values (e.g. voltage and resistance or voltage and current).
  2. Click the "Calculate" button.
  3. The calculator will automatically fill in the remaining fields, applying the appropriate formulas.

You don't have to remember which formula to apply in a given situation - the tool does it in the background, reducing the risk of calculation errors and speeding up daily work.

Practical applications of the calculator

The Ohm's Law calculator is a universal tool that will be useful in both simple experiments and in designing more complex systems.

Example applications:

  • Selection of resistors, e.g. to limit the current of an LED diode, set the operating point of a transistor, create a voltage divider.
  • Estimating load current when we know the supply voltage and the resistance of the receiver (heater, bulb, coil).
  • Calculating power lost on elements to select the appropriate power resistor or radiator for the power circuit.
  • Verification of the power supply project, i.e. checking whether the power supply has an adequate current and power reserve for all receivers.
  • Diagnosis of faults, if an element heats up more than would result from calculations, the calculator helps to quickly compare theory with the actual behavior of the system.

In combination with the catalog notes of components, the Ohm's Law calculator provides practical support in the daily work of electronics engineers, automation engineers and hobbyists.

FAQ - Frequently Asked Questions about the Ohm's Law Calculator

Why do I need at least two values to calculate something?

Ohm's Law and power formulas connect four quantities: voltage (V), current (I), resistance (R) and power (P).

Each equation has two known and one sought (e.g. V = I × R - to calculate V, you need to know I and R). If you provide only one value, the system of equations is "underdetermined" - there are infinitely many combinations of the remaining parameters. Therefore, the calculator requires a minimum of two numbers to be able to unambiguously calculate the rest.

Can the calculator be used for alternating current (AC) calculations?

Yes, but with a few reservations.

For simple resistive loads (e.g. pure heater, resistor, classic bulb) Ohm's Law works the same as with DC - provided that you use effective values of voltage and current (e.g. 230V AC).

For circuits with coils and capacitors (inductance, capacitance) reactance and phase shift are added - then the usual V = I × R is not enough and the concept of impedance must be used. The calculator can be treated as an approximation only for the "purely resistive" part.

How to interpret the results if the calculator shows a very high current?

A very high current in calculations usually means that the resistance entered into the calculator is very small compared to the supply voltage.

This may mean:

 
a real short circuit or almost short circuit in the planned system (e.g. forgotten resistor, too low resistance),  or simply an error in the input data, e.g. a mistake in units (mΩ instead of Ω).

If the calculator shows a current significantly exceeding the capabilities of the power supply or elements, it is worth assuming that such a system in practice is dangerous and requires correction (addition/greater resistance, voltage limitation, protection).

How to check with the calculator whether a fuse with a specified current will work at a given voltage and load?

  1. Enter the supply voltage and known load resistance (or voltage and power).
  2. Read the load current (I) from the calculator.
  3. Compare the obtained current with the nominal current of the fuse:
    • if the load current is lower than the nominal current of the fuse - the fuse should not work under normal conditions,
    • if it is higher - the fuse will work (depending on the characteristic: fast/delayed).

Remember that fuses have their own time-current curves. A slight exceedance of the nominal current may cause operation only after a longer time, and a large exceedance - very quickly.

Can I use the calculator to estimate how a change in supply voltage will affect the current and power of elements?

Yes - this is one of the simplest applications.

  • First, calculate the system for the first voltage (e.g. 12V) - enter the voltage and resistance, read the current and power.
  • Then change only the voltage in the calculator (e.g. to 9V) and read the new values.

For purely resistive load:

  • current changes proportionally to voltage (I ~ V),
  • power changes with the square of the voltage (P ~ V²).

So a drop from 12V to 9V is ¾ of the voltage, but the power will drop to (9/12)² = 0.56… ≈ 56% of the original value.

How does the calculator help to select resistor values in a voltage divider?

The calculator itself does not "design" the divider, but helps to calculate:

  1. The current flowing through the divider - you enter the supply voltage and the equivalent resistance (R1 + R2 for a series divider), you read the current.
  2. Power losses on each resistor - for a given current you can calculate the power P = I² × R on R1 and R2.

Typical procedure:

  • you initially select R1 and R2 from the simple divider formula (Uout = Vin × R2 / (R1 + R2)),
  • in the calculator you check the divider current and power on the resistors,
  • if necessary, increase the resistances (less current) or power of the resistors (greater reserve).

This makes it easy to avoid situations where the divider draws unnecessarily high current or has too small power resistors.

Does the calculator take into account the fact that the resistance of elements can change with temperature?

No - the calculator assumes constant resistance, exactly as you enter in the R field. In reality, many elements (resistors, wires, heaters) have a temperature coefficient, so their resistance increases or decreases with temperature. In typical, low-power systems, differences are small and can be ignored. However, at high powers and high temperatures, data from the catalog note (TC, TCR) must be taken into account and the resistance value must be corrected independently if necessary.

Does the calculator take into account voltage drops on wires and connectors, or should they be added separately?

The calculator operates on the voltage that you provide as the input value. If you want to take into account voltage drops on wires, connectors or other elements, you must:

  • either enter the actual voltage on the load into the calculator (i.e. the power supply voltage minus drops),
  • or calculate (e.g. separately) the resistance of the wires and include it in the total resistance of the system.

In other words - the calculator does not "know" about wires and connectors until you include them in the input data.

Can I use the calculator if I know the voltage and power, but I don't know the current or resistance?

Yes - this is a common case and the calculator handles it perfectly.

If you know:

  • voltage V
  • power P

you can determine:

  • current: I = P / V
  • resistance: R = V² / P

In practice:

  1. Enter V and P into the calculator.
  2. The tool itself will calculate I and R based on the above relationships.

This is useful e.g. when you have a heater or bulb described as "12V / 10W" and you want to know what current it draws and what its effective resistance is.

Did you know that...

  • Ohm's Law was once unpopular. Georg Ohm published his research in 1827, but the scientific community received it very coolly. It was considered "too theoretical" and not very practical. Only after years it turned out that without this law it is hard to imagine modern electrical engineering.
  • Ohm's Law does not apply "everywhere and always". Resistors, wires, heaters - behave according to the theory, i.e. they fulfill V = I·R. But already LED diodes, halogen bulbs, transistors or saturating elements - are not linear elements and the classic Ohm's Law applies to them only locally or approximately.
  • Ohm's Law is often the first "filter" of common sense in the project. If it turns out from the calculations that at 5V and "almost zero" resistance, several hundred amperes flow - it is a sign that the system is practically a short circuit. Many designers use Ohm's Law simply to catch such absurdities at the sketch stage.
  • Ohm's Law is often also the first test of the correctness of units. If you enter voltage in volts and current in milliamperes, without conversion, the result R will come out "from space". Many engineers first check: "does the order of magnitude make sense" before they believe in the result.
  • A resistor that heats up slightly usually works "happily". If from Ohm's Law and the formula for power it turns out that the resistor works e.g. at 30-50% of its nominal power, then slight heating is normal. Completely cold with large calculated losses may mean that... no current flows through it at all, because the system is interrupted.
  • Formulas for power can save a component from "frying". Often the project starts from functions, and only then someone counts: P = I²·R or P = V²/R and suddenly it turns out that a small, inconspicuous resistor would have to dissipate 2-3W. This is the moment when the Ohm's Law calculator saves burnt PCB.

READ ALSO