+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

HENSEL

HENSEL is a German manufacturer and supplier of electrical installation solutions with nearly 100 years of experience. The company manufactures innovative products serving for the implementation of power and control systems in industry, construction, power engineering and many other fields of the economy. Since its founding (in 1931), HENSEL has placed emphasis on growth, and today, it offers customers products that support the ergonomy and ecology of industrial systems and sustainable development, alongside a series of renewable energy source solutions, such as products for photovoltaic panel installation and energy storage.

Housings and cable accessories were the first products from the HENSEL portfolio to enter the TME catalog. The former include, above all, electrical installation elements (so-called boxes), distinguished by a high protection rating, which, in most cases, reaches or exceeds IP66, i.e. full dust-tightness and resistance to pressurized streams of water. This means that products can not only be used outdoors but also cleaned by means of pressure washers, while constantly protecting the cables, terminal blocks, etc. placed inside. The manufacturer produces articles in the scope of fire safety installations, universal housings (for implementation of one-time or low-budget projects), as well as a broad range of accessories (pressure-compensating pass-throughs, descriptive plates, holders, etc.). What is more, screw terminals and universal glands with a broad range of diameters compatible with the housings can be purchased with TME.