+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

MOLEX

Molex is one of the most recognizable brands in the connector industry. This American company, which traces its history back to 1938, has become a trustworthy name over the course of the 20th century, building its reputation on superior electronic and electrical connection solutions. Today, the brand's mission is much broader than just producing proven and durable solutions. The supplier focuses on the development of communication technology, medical technology, and other areas that have a direct impact on the quality of our lives. The manufacturer's specialized connectors are used not only in computers or industrial devices, but also in hearing aids, 5G data communication systems, home automation, and many other applications directly related to the progress of modern electronics. Molex also focuses on production without any negative impact on the environment. Thus, the supplier's connectors are compliant with numerous international standards.

Molex offers almost all types of connectors. These are simple, signal connectors with a pitch of 1 mm to 10 mm, including pin headers, etc. They also include IDC and FFC (ribbon) connectors - typically used for signal transmission in electronic devices of various types, from the simplest household appliances and electronics to industrial controllers and precision electronics (e.g., measuring instruments). In the industrial field, Molex connectors are characterised by their resistance to mechanical agents and tightness. These include circular (M8, M12, 7/8" etc.) and rectangular HDC connectors. In the latter group, Molex supplies modular products (polymer inserts, metal bodies) and accessories for them, such as gaskets and multi-element glands protecting contacts from corrosive elements. The manufacturer also supplies typical connectors for data transmission, such as USB, D-Sub and RJ connectors - products commonly used in information and communication systems. A lesser-known area of Molex's business activity is the manufacture of enclosures. Their characteristic feature is the IP66 rating and the manufacturing material (aluminium). The features of these solutions allow them to be used in industrial conditions, even outdoors and in plants or machines, where they will be exposed to dust, vapours, low / high temperatures, etc.

When deciding to purchase Molex products, customers can be sure that they are choosing the best possible solution: designed by top-class engineers - with ergonomics, progress and long-term performance in mind.

Products

View manufacturer's products