+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

RADPOL

RADPOL S.A. – a company that specialises in manufacturing heat-shrink products, mainly made of heat-resistant polyethylene, produced with the use of original material blends. In addition, the company offers multi-layered sewer, water supply and gas pipes, as well as elements which are used in the manufacture of heating systems. This wide portfolio is a perfect proof of RADPOL’s commitment when it comes to the development of its manufacturing capacity and rich technological facilities.

The first group of RADPOL products which has joined the TME catalogue includes heat-shrink tubes, one of the most basic accessories for electrical and electro-technical engineers; commonly used in workshops, service centres, as well as in the production of machines, household appliances, audio/video devices or vehicles. The manufacturer offers protective items with the shrink ratio of 2:1, 3:1 and even 4:1, in various diameters and colours. Most of them are available in 1 m segments, but they can also be purchased in reels (50 m or 100 m) . What makes these products special are their thin walls covered with an adhesive and made of a flexible material.