+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
The anode is the electrode into which electrons flow from the external electrical circuit. Depending on the type of device or electrochemical process, it can function as either the positive or the negative terminal. In general terms, the anode is the site at which oxidation occurs—that is, where particles or ions release electrons—making it a critical component in electrochemical cells, vacuum tubes, semiconductor diodes, and many other systems.
In a galvanic (voltaic) cell, the anode serves as the negative terminal because it supplies electrons to the external circuit. Conversely, in an electrolytic cell, the anode is the positive terminal that attracts anions from the electrolyte. In vacuum devices, such as electron tubes or cathode ray tubes, the anode attracts electrons emitted by the cathode and is typically positively biased with respect to it. In semiconductor diodes, the anode is the terminal to which a positive voltage must be applied relative to the cathode in order to allow current to flow.
The significance of the anode extends beyond simple conduction—its material, geometry, and operating conditions influence the durability, efficiency, and performance characteristics of the entire system. In electrical engineering and industrial chemistry, the selection of a suitable anode is essential for technological processes such as electroplating and electrolysis, as well as for the design of energy sources like batteries and fuel cells.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.