+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Bandwidth - definition

Bandwidth is the range of frequencies over which a signal, transmission system, or electronic component effectively transmits or processes energy. It refers to the difference between the upper and lower frequency limits within which the signal level remains within a specified range—typically defined as a 3 dB drop from the maximum amplitude. This quantity is expressed in hertz (Hz) and is a key criterion for evaluating a system’s ability to accurately convey information.

In telecommunications, bandwidth defines the amount of information that can be transmitted through a channel per unit of time. The wider the bandwidth, the higher the data throughput and the ability to transmit more complex or faster signals. In electronics, bandwidth is used to characterize amplifiers, filters, antennas, and measurement systems, determining the frequency range over which the component operates effectively.

From a signal theory perspective, limited bandwidth affects the shape and fidelity of complex signals. In digital systems, it directly relates to sampling frequency and the ability to reconstruct signals according to the Nyquist theorem. In engineering practice, it is crucial to match the bandwidth to the nature of the signal, avoid aliasing effects, and suppress interference outside the usable frequency range.

In both wireless and wired transmission systems, bandwidth is a limited resource subject to legal regulations and frequency planning. The allocation of frequency bands for specific applications—such as mobile communications, satellite systems, or radar—is governed by international and national standards. Effective bandwidth management is essential for the reliable operation of modern communication systems and information infrastructure.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO