+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Absolute zero - definition

Absolute zero is the lowest possible temperature in nature, at which matter’s molecules reach their minimum energy state and all thermal motion ceases in the classical sense. In the Kelvin scale, this corresponds to 0 K, which is equivalent to –273.15°C on the Celsius scale. This temperature represents the lower limit of the absolute temperature scale and serves as a fundamental reference point in many fields of physics, including thermodynamics, cryogenics, and solid-state physics.

According to classical mechanics, as a substance approaches absolute zero, the vibrational motion of its atoms and molecules comes to a near standstill, resulting in the lowest possible internal energy. However, quantum mechanics dictates that even under such extreme conditions, particles retain so-called zero-point energy due to Heisenberg’s uncertainty principle, which implies that a complete “freezing” of matter is not physically attainable.

Although absolute zero cannot be reached in practice, modern experimental techniques allow physical systems to be cooled to mere fractions of a nanokelvin above this limit. At such ultra-low temperatures, macroscopic quantum phenomena emerge, such as Bose–Einstein condensation and superconductivity, where particles behave collectively as coherent systems with precisely defined properties.

In thermodynamic terms, absolute zero is associated with the third law of thermodynamics, which states that the entropy of a perfect crystal approaches zero as the temperature approaches absolute zero. This concept plays a critical role in defining temperature units and in the analysis of energy processes and material properties at extremely low temperatures. Absolute zero is also the point at which various temperature scales, such as Kelvin and Rankine, converge to zero, forming a universal basis for thermal measurement.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO