+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Buffer - definition

Buffer is a technical term referring to a component that mediates the flow of data or signals between two systems, systems or processes that operate at different speeds, capacities or modes of operation. The main function of a buffer is to temporarily store data so that synchronisation of transmission between source and receiver is possible, minimising information loss and optimising system operation.

In IT, a buffer is a specially allocated space in the operating memory where input or output data is stored during processing. Such a solution reduces delays and increases the efficiency of I/O (Input/Output) operations, e.g. when reading files, transferring audio/video streams or communicating with external devices. Buffers are also important in network transmission, where packet data must be processed with order and integrity.

In electronics, the term buffer can also refer to logic circuits that amplify a digital signal without altering it logically. Such circuits provide load separation from the signal source and improve the reliability of information transfer in complex digital systems. Buffers are also used in the context of analogue circuits, where they perform the function of matching impedance or isolating circuits.

Depending on the application, the buffer can be in hardware or software form. In operating systems, buffering mechanisms are used to improve the efficiency of storage media, Mass Storage and peripherals. In real-time system design, buffer management plays a key role in ensuring deterministic system response. The correct choice of buffer size and its emptying strategy (e.g. FIFO - First In, First Out) directly affects the stability and speed of the entire system.

Buffers, transceivers, drivers

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.