+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

DML (Data Manipulation Language) - definition

DML (Data Manipulation Language) is a subset of SQL (Structured Query Language) for operations on data stored in relational databases. Its main purpose is to allow the user to add, modify, delete and read records in tables without interfering with the structure of the database itself. DML operates at the level of content rather than schema definition and therefore plays a key role in the day-to-day use of database management systems.

DML instructions are executed in a transactional context, meaning that changes made using them can be approved (commit) or rolled back (rollback), ensuring data integrity even in multi-user environments. These operations are fundamental to the integrity and timeliness of information in information systems, and their correct use is important in the design of applications using databases.

The DML language allows precise filtering of data using logical conditions and comparison operators, supporting the creation of dynamic and flexible queries. Its syntax is designed to reflect the natural language of end-user queries, facilitating the work of database administrators and developers alike.

In the context of relational databases, DML often co-exists with other subsets of SQL, such as DDL (Data Definition Language), responsible for creating and modifying data structures, and DCL (Data Control Language), which manages access permissions. The role of DML, however, focuses exclusively on the manipulation of the data itself, making it one of the most operational and practical tools in the day-to-day operation of database systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO