+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Isolation - definition

Isolation is the property of a material or structure to restrict the flow of energy, particles or information between separated areas. Others use the term in a technical context with different meanings depending on the field - it includes electrical, thermal, acoustic, vibration or electromagnetic insulation, among others. The purpose of using insulation is to ensure safety, improve energy efficiency, protect sensitive components or separate signals.

In electrical engineering insulation refers to the use of electrically non-conductive materials to prevent current flow between conductors, circuits or components. Insulating materials, such as plastics, ceramics, glass or electrical insulating oils, protect against short circuits, paralysis and degradation of equipment under the influence of operating voltages and surges. The quality of insulation is determined, among other things, by its dielectric strength, volume resistivity and resistance to environmental conditions.

In mechanical engineering and construction, thermal insulation limits heat transfer between spaces of different temperatures. It is used to protect against energy losses and to stabilise the operating conditions of equipment and rooms. In acoustics, on the other hand, insulation serves to dampen noise and limit the propagation of sound waves. In Automation and Electronics it is also important to use galvanic isolation - electrically separating different parts of a system while allowing signal transmission via transformers, opto-isolators or capacitive coupling.

The selection of the appropriate type and level of insulation depends on the physical parameters of the operating environment, the required durability, temperature range, voltage, frequency and safety standards. Properly designed insulation has a direct impact on the reliability, durability and functionality of technical systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO