+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
The Logarithm is a mathematical function that is the inverse of power, which allows us to determine the exponent of the power to which a given base must be raised to obtain a given number. Formally, the logarithm of a number x with base a (where a > 0 and a ≠ 1) is called such a number y for which the equality a^y = x holds. This is written as logₐ(x) = y.
The primary use of the logarithm is to simplify operations on large numbers by transforming multiplication into addition, division into subtraction, and multiplication into triplication. Due to these properties, logarithms played an important role in the development of computational mathematics, especially before the era of calculators and computers, finding use in logarithmic sliders and computational tables, among others.
Others types of logarithms are used in mathematics and technical sciences, depending on the choice of base. The decimal logarithm, denoted as log(x), has a base of 10 and is commonly used in engineering and physics. The natural logarithm, denoted as ln(x), has base e (Euler's number) and is common in mathematical analysis and modelling of exponential processes. In computer science and information theory, the logarithm with base 2, written as log₂(x), is used because it corresponds to the binary structure of the data.
Logarithms play an important role in many fields, including the analysis of signal scales (e.g. decibels (dB) in acoustics and telecommunications), modelling of non-linear phenomena, complexity theory of algorithms and data transformations in statistics and machine learning. Their mathematical properties, such as monotonicity and continuity, make them useful tools in function analysis and differential equations.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.