+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Multiplexing (multiplexing) - definition

Multiplexing, also known as multiplexing, is a technique used in telecommunications, transmission and digital systems to efficiently transmit multiple signals over a single transmission medium, while maintaining the integrity of the individual data streams. This process allows multiple channels of information to be transmitted simultaneously by appropriately separating them in the frequency, time, wavelength or coding domain.

In classical telecommunications, multiplexing is divided into several basic types: frequency-domain multiplexing (FDM), time-domain multiplexing (TDM), coding-domain multiplexing (CDM) and spatial-domain multiplexing (SDM). Each of these techniques relies on a different signal separation mechanism to make optimal use of the available channel bandwidth and minimise interference. For example, in FDM systems, individual signals are transmitted on different frequency bands, while in TDM different time slots are allocated within a common channel.

In modern communication networks, such as fibre-optic systems (WDM - Wavelength Division Multiplexing), multiplexing allows hundreds of channels of data to be transmitted over a single beam of light, significantly increasing system throughput. In digital systems, multiplexers are integral components of integrated circuits and microprocessors, enabling the selective transmission of data from multiple sources to a single receiver.

Multiplexing is used in a wide range of technologies, from mobile telephony and broadband internet, to digital TV broadcasting systems, to radar systems and satellite communications. The high efficiency of data transmission, reduced infrastructure costs and increased flexibility in managing transmission resources make multiplexing a fundamental technique for modern communication and information systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO