+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Capacity - definition

Capacity is a general technical term referring to the maximum capacity of a given system, device or process to process, transmit or transport a given amount of resources per unit time. Depending on the technical context, it can refer to different fields such as data transmission, systems engineering, Automation, logistics or signal processing. It is most often expressed in quantitative units per second, e.g. bits per second for digital data, units of volume in flow systems or number of operations in computing systems.

In communication systems, throughput describes the maximum amount of data that can be transmitted over a channel or network in a given amount of time, regardless of any interference or loss. In the context of computer systems, it can refer to the ability of a processor, bus, Interfaces input/output or memory to handle a specific stream of information. In Automation and Mechanical Engineering, on the other hand, the term refers to the performance of production lines, conveyors, valves or pumping systems.

From a technical point of view, system throughput is sometimes limited by physical components, transmission delays, interference, design parameters and control algorithms. Its optimisation is an important issue in system design, as it directly affects efficiency, response time, reliability and economy of operation. In practice, throughput can be time-varying and depend on current system operating conditions, configuration and load.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO