+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

SPI (Serial Peripheral Interface) - definition

SPI (Serial Peripheral Interface) is a synchronous communication interface designed to exchange data between a microcontroller and peripherals in electronic systems. The standard was developed by Motorola and is widely used in applications requiring high-speed, full duplex information transfer with a small number of transmission cables.

The SPI interface is based on the principle of serial bus operation with one master and one or more slaves, requiring an individual chip select line for each slave. Communication is via four basic signals: the transfer clock (SCLK), the data sent by the master (MOSI), the data sent by the slave (MISO) and the chip select signal (SS or CS). Transmission synchronisation allows precise control of data flow and elimination of errors due to the absence of a reference clock, which distinguishes SPI from asynchronous interfaces.

SPI has the advantage of simplicity, low latency and high bandwidth, making it suitable for Flash memories, ADC/DACs, displays or sensors. However, the interface does not include mechanisms for addressing or multi-device automated transmission, which limits its use in more complex network topologies. The configuration of the SPI protocol can be customised in terms of operating mode, clock polarity and sampling phase, providing flexibility to suit the requirements of different circuits.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO