+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Synchronisation - definition

Synchronisation is the process of bringing two or more signals, processes, devices or systems to a common rhythm, phase or reference point in time. In technology, it means ensuring temporal consistency between activities occurring in parallel, independently or at different locations. Synchronisation is a key issue in many fields such as digital electronics, telecommunications, Automation, computer science and real-time systems.

In digital systems, synchronisation refers to the alignment of clock signals to ensure correct data transmission between different logic modules. Incorrect synchronisation can lead to misalignment, data loss or transmission interference. In Computer Networks and telecommunication networks, it refers to the temporal correspondence of data transmission between nodes, which allows the data to be correctly decoded, analysed and further processed. Clock synchronisation protocols and mechanisms such as NTP (Network Time Protocol) or PTP (Precision Time Protocol) are crucial in this respect.

In dynamic and control systems, synchronisation refers to the convergent operation of multiple systems relative to a common timing pattern, allowing complex tasks to be performed in a synchronised and coordinated manner. In robotics and mechatronics, synchronisation is essential in the operation of multi-axis drive systems, and in power generation, in connecting generators to the power grid without causing phase and frequency disturbances.

Synchronisation can be implemented in hardware, through clock lines and reference signals, or in software, through timing algorithms and logic states. Clock drift correction and transmission delay compensation methods are also often used. In distributed systems, where there is no common time source, synchronisation is a prerequisite for data consistency and deterministic events.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO