+13,00,000 products in offer

6,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Sensor - definition

A sensor is a component of a measurement or control system designed to detect a specific physical or chemical quantity and convert it into a signal suitable for further processing. This signal may be electrical, optical, pneumatic, or digital, depending on the applied technology and the type of measured variable. Sensors play a crucial role in automation, robotics, consumer electronics, medicine, and safety systems by providing data essential for decision-making and control.

The operating principle of a sensor is based on the response of its structure or active material to environmental changes, such as temperature, pressure, motion, light intensity, the presence of chemical substances, or electromagnetic fields. This response is then converted into a measurable signal by an appropriate processing circuit. In modern systems, sensors are often integrated with signal conditioning electronics, digital interfaces, and data analysis algorithms, enhancing their precision and functionality.

In engineering, sensors represent the first stage of the measurement chain and have a direct impact on the overall accuracy and reliability of a system. Proper sensor selection depends on the required performance parameters, such as measurement range, resolution, response time, and resistance to environmental conditions. In automated systems, sensors provide real-time information about the state of a process or its surroundings, enabling dynamic adaptation of machine, device, or installation behavior.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO