+13,00,000 products in offer

6,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Cache memory - definition

Cache memory is a high-speed semiconductor memory with limited capacity, used for temporarily storing the most frequently accessed data and instructions to enhance the performance of a computer's central processing unit (CPU). Its primary purpose is to reduce the latency associated with accessing slower main memory (RAM) or other data sources such as mass storage devices. Due to its physical proximity to the processor and significantly shorter access time, cache memory enables faster data processing and alleviates the so-called bottleneck effect in computer systems.

Cache operation relies on the principle of locality of reference—both temporal and spatial. Temporal locality assumes that data recently accessed is likely to be accessed again soon, while spatial locality suggests that data located near recently accessed information is also likely to be needed. Based on these assumptions, cache systems implement predictive algorithms to determine which data should be retained and which can be discarded to make space for new entries.

Cache memory is typically organized into multiple levels: L1 (closest to the CPU core, smallest and fastest), L2 (larger but slower), and L3 (shared across multiple cores, with the highest capacity and lowest speed among cache levels). These levels function hierarchically, allowing for efficient data flow between the processor and other system components. In the event of a cache miss, where the requested data is not found in the cache, the processor must access a lower cache level or main memory, resulting in increased latency.

Cache plays a crucial role in the performance of computer systems, microprocessors, controllers, and embedded devices. Modern processor architectures incorporate advanced cache management mechanisms, including data prefetching, coherence protocols, and replacement policies, all aimed at maximizing cache hits and minimizing access time. In specific applications such as servers, real-time systems, or graphics processing, optimizing cache memory is a key aspect of system design.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO