+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Raspberry Pi SSDs and SSD Kits

Date of publication: 20-05-2025 🕒 2 min read

Do you own a Raspberry Pi 5 and want to unlock its full potential? Check out new accessories by Raspberry Pi. The brand has launched their own NVMe SSDs that you can purchase separately or as ready-to-use SSD Kits with the M.2 HAT+.

Raspberry Pi 5 was launched about a year ago and was a great success for the producer. It has brought many new features and improvements, such as a 3x increase in performance compared to the previous model, Raspberry Pi 4 from 2019, as well as a power button and PCI Express port.

The PCI Express port can be used with different external accessories, for example AI accelerators, Ethernet adapters, or regular PC graphics cards. Raspberry Pi offers the affordable M.2HAT+ of their own production, which you can use for conversion from their FPC standard to the M.2 M-key format. There is also quite a lot of third-party adapters that can achieve similar results, but we recommend using the official producer’s accessories, such as Raspberry Pi AI Kit that combines the M.2 HAT+ with a Hailo AI inference accelerator, and the newer Raspberry Pi AI HAT+.

However, the most popular application the PCI Express port is used for, is attaching an NVMe solid-state disk (SSD). SSDs are a great choice, since they’re even faster than the A2-class SD cards. If you want the best possible performance, we recommend running Raspberry Pi OS from an SSD, and Raspberry Pi’s SSDs are just perfect for this.

The drives are available in the 256GB and 512GB versions. They both offer minimum 4KB random read and write performance of 40k IOPS (256GB version) and 70k IOPS (512GB version). They provide an effective an affordable way to help your Raspberry Pi 5 achieve the highest possible level of performance.

Note: This article is based on original content from: https://www.raspberrypi.com/news/raspberry-pi-ssds-and-ssd-kits/

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO