+13,00,000 products in offer

6,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Microcomputer - definition

A Microcomputer is a type of digital computer whose primary computing element is the microprocessor - an integrated circuit containing the central processing unit (CPU). It emerged from the development of microelectronics and represents one of the most important achievements in the miniaturisation of computer technology. Microcomputers integrate not only the CPU, but also the operating memory, input-output circuits and often the data storage and communication interfaces in a single enclosure, making them functionally self-contained computing units.

The term became widespread in the 1970s with the advent of the first personal computers, which made information technology accessible to a wide range of users. Unlike computers mainframe and minicomputers, microcomputers are small, energy-efficient and designed for individual or embedded use.

From an architectural perspective, microcomputers can run under a variety of operating systems or as system-less (bare-metal) systems, particularly in embedded applications. They are used extensively in Automation, robotics, consumer devices, and as educational and prototyping platforms. Today, many come in the form of development boards, such as the Raspberry Pi, offering a wide range of functionality while maintaining a compact form factor.

A microcomputer is not the same as a microcontroller - although both use microprocessors, a microcontroller integrates additional peripherals and often operates in purpose-built environments. A microcomputer, on the other hand, enables more complex tasks, including multitasking, data processing and running extensive software.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO