+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Date of publication: 11-09-2024 Update date: 10-04-2026 🕒 6 min read
Does clock construction always require masterful precision? Discover how to build a functional and eye-catching clock using 3D-printed elements and Arduino..
Download the STL files here >LINK<. Use your 3D printer or a 3D printing service to manufacture all the necessary components. This may take some time. :)Be sure to print the caps in a different colour than the rest of the project, to ensure that the digits can be distinguished from the rest.
Assemble the components for the digits by mounting the 28 Micro Servo motors onto each base plate, as shown in the picture to the right..
Mount the 28 single 3D-printed segments onto each one of the Servo Motors.
Ensure that the segments are aligned as shown in the picture below.
Place the 28 differently colored 'shoes' onto the 28 segments. To improve the quality of the shoes, you may consider 3D-printing them at a higher quality. The print quality of the ones used in this project were 0.2 mm.
Assemble the frame of the mechanical servo clock. The parts can be clipped together, but for improved stability, you can use some bolts and nuts.
Insert the individual digits into the outer frame, paying attention to the top and bottom of the digits. Ensure that all four digits are mounted in the same direction.
Connect the 28 micro servo motors to the two PCA9685 Drivers, as shown in the schematic image below. You may need to zoom in to read the connection numbers (0-15).
To identify the servo motors, refer to the second image where the arrangement is shown.
Solder a connection from the A0 bridge to the second PCA9685 servo driver. Then, connect both drivers together as shown in the schematic image above.
Connect the PCA9685 driver to the Arduino using an I2C connection. SCL should be connected to Pin A5, and SDA should be connected to Pin A4 of the Arduino UNO. Also, connect the driver to the GND and 5V pins of the Arduino.
Add a external power supply to ensure sufficient power for the 28 servo motors. Connect the external power supply to the Arduino by establishing a connection between GND and connecting the output voltage to the VIN Pin of the Arduino.
Connect your Arduino to your PC and open the Arduino IDE. Download the Code and upload it to the Arduino UNO.Here is the link to the Code: >>LINK<<
Disconnect the Arduino from the PC and power it only from the external power supply. Enjoy!
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.