+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Remote sensing is a field of technology and science dealing with the acquisition of information about objects, phenomena or surfaces without direct physical contact with the area under study, using electromagnetic waves. The process involves recording the radiation reflected, emitted or scattered by a target object using sensors placed on remote platforms - such as satellites, drones, aircraft or ground-based devices - and then analysing the resulting data to identify and classify the observed features.
In practice, remote sensing covers a wide spectral range - from visible radiation, infrared, to microwaves and radio waves. Others ranges allow the observation of physical and chemical properties of surfaces, such as temperature, humidity, structure, material composition, vegetation or contamination. Sensor calibration and signal processing for geometric, atmospheric and radiometric correction is an important element, allowing reliable measurement data to be obtained.
Remote sensing is divided into passive and active - in the first case, the sensor records natural radiation (e.g. sunlight), while in the second it uses its own emission source, e.g. radar or lidar, which generates a signal and analyses its reflection from the surface. The technique has a wide range of applications in environmental monitoring, precision agriculture, geology, hydrology, land use planning, military, meteorology, and emergency management, e.g. in assessing the effects of natural disasters.
The interpretation of remote sensing data requires advanced computational tools, classification algorithms, image segmentation methods and spatial information systems (GIS). Modern remote sensing uses artificial intelligence and machine learning technologies to automatically analyse images and detect changes over time, which significantly increases its efficiency and range of applications.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.