+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

HDMI - definition

HDMI (High-Definition Multimedia Interface) is a digital interface used for transmitting uncompressed audio and video signals between multimedia devices. Developed in the early 21st century by a consortium of consumer electronics manufacturers, the standard serves as a universal solution for high-definition video and multichannel audio transmission, eliminating the need for multiple separate cables. HDMI enables data transfer via a single cable, simplifying connections and improving both the aesthetics and reliability of installations.

The HDMI connector supports video transmission in HD, Full HD, 4K, as well as 3D and HDR formats, depending on the protocol version and hardware capabilities. The interface also supports Audio Return Channels (ARC, eARC), EDID data for automatic display parameter configuration, and HDCP digital content protection to safeguard intellectual property. HDMI is fully compatible with image synchronization technologies, allowing for smooth playback without latency or interference.

HDMI technology is widely used in consumer electronics, computers, gaming consoles, projectors, monitors, and home theater systems. Different versions of the interface offer varying bandwidths, supported resolutions, refresh rates, and additional features. Due to its versatility and ongoing development, HDMI has become the industry standard, supported by the majority of electronic device manufacturers. Its digital nature ensures high signal quality and resistance to interference, making it a core solution in next-generation audiovisual systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO