+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Bridge rectifier – what is worth knowing about it

Date of publication: 28-01-2025 Update date: 10-04-2026 🕒 6 min read


The rectifier bridge is an extremely important electronic component that, when combined with a filtering capacitor, creates a power or charging system available in every home. The correctness of its operation directly affects the quality of power supply to electronic devices, and consequently, their lifespan. Basic knowledge of diagnosing or even independently constructing rectifier bridges can prove very useful. In the article, we will describe these components, present their construction and operation method.

Why must the voltage from the socket be transformed?

The primary goal of the power plant is to effectively and as cheaply as possible deliver the electricity produced at the power plant to all customers. The continuous flow of electrical charges through power networks is associated with significant losses. These are related to the dissipation of energy into the environment in the form of generated heat. We can limit the effects of such a phenomenon by increasing the electrical voltage in the network. Based on many experiments and calculations, it has been accepted that the most efficient form of electricity transmission is closely related to the use of alternating voltage for this purpose. High voltage, which allows the transmission of alternating current over hundreds of kilometers to the most distant consumers, is then reduced using power transformers. It has also been accepted that the voltage that will effectively and relatively safely power electrical devices in households is 230V.

So, is the alternating voltage currently present in a standard electrical socket suitable for every application? The answer is no. This is why the use of a rectifier bridge is an extremely important solution.

Rectifier bridge – what function does it serve?

We encounter a rectifier bridge wherever the powered device requires appropriately adjusted voltage and direct current. Such a power supply method is used by electronic devices. The bridge is a relatively small electronic component used in power supplies or chargers, which are the direct transmitters of electrical energy between the socket and the powered device. Despite its unassuming appearance, without a rectifier bridge, it would be impossible to start a computer or other devices requiring power from battery chargers or power supplies.

Construction of the rectifier bridge

One of the most popular rectifier bridges is the Graetz bridge, a full-wave, single-phase rectifier equipped with four independent rectifying diodes (or in the form of an integrated circuit), which, connected in the appropriate configuration, fully utilize the wave of the supply voltage to deliver a specific power to the receiver in the form of direct current. Rectifier bridges are available in various housings. Plastic (for low-voltage) and metal (for bridges operating at higher currents or voltages) are most commonly used. To fulfill its task, two of the four connectors are responsible for voltage regulation and are connected to the alternating voltage source. The other pair forms a connection with the device powered by direct current. To obtain additionally filtered output voltage from the bridge, the rectifier circuit is connected to a capacitor, whose task is to smooth the voltage.

Principle of operation

In each half of the period, only one pair of diodes is responsible for conducting electric current. It works in the forward direction, while the other pair is polarized in the reverse direction. When the direction of current flow changes, the pairs switch tasks, and the diodes responsible for conduction are polarized in reverse. A capacitor in such a system allows for the reduction of ripple levels through meticulous voltage filtration at the output. The Graetz bridge has high efficiency, and consequently, it is used in many single-phase systems.

Basic parameters of rectifier bridges

Before we start connecting the rectifier bridge to the electrical system, we must first analyze the available device variants and, based on the nominal parameters, choose the appropriate solution for the intended application.

The solutions available on the market are characterized by the following parameters:

  • Maximum forward current If [A] – indicates the maximum current value that the rectifier can safely conduct without the risk of overheating and damaging the system. The sensitive elements of the bridge are silicon diodes, which can simply be damaged if the critical temperature is exceeded;
  • Maximum reverse voltage VRRM [V] – similarly, the maximum reverse voltage is the limit of safe operation without the risk of damaging the rectifier bridge. This time, however, we are talking about the peak voltage accompanying the system's operation in the reverse direction;
  • Operating temperature Tj [°C] – the operating temperature concerns the safe range for which the rectifier bridge will not be exposed to overheating or damage to the materials from which it was made due to too low a temperature;
  • Reverse current IR [A] – this is the maximum allowable current intensity value that flows during operation in reverse polarization;
  • Dimensions and construction – rectifier bridges find their application in many solutions. To select the appropriate specimen, it is often necessary to consider the construction and the possibility of placing the element in a very tight housing. Manufacturers of rectifier bridges offer a wide range of available constructions;
  • Type of bridge (single-phase, three-phase) – to properly select the type of bridge for the electrical system, it is necessary to familiarize oneself with the installation itself. There are single-phase solutions, i.e., popular Graetz bridges, used in single-phase systems. There are also multi-phase bridges, which are an extended form of the aforementioned, as three parallel branches with Graetz bridges. They are dedicated to multi-phase systems.

Connecting the rectifier bridge to the electrical system

Two diagonally located connectors are used to connect the rectifier bridge to alternating voltage. It is then transferred from the secondary winding of the transformer to the diodes of the Graetz bridge. The other two connectors are responsible for outputting the rectified voltage. The connection of the bridge with the transformer system is made using electrical wires. Such a simple system, based solely on the rectifier bridge, would generate a signal burdened with a large amount of ripple and distortion. To avoid this, an additional filtering system is used, in which the capacitor influences the removal of unwanted deviations. Additionally, to obtain a stable voltage value, especially important in the case of sensitive electronic systems in modern receivers, a voltage stabilizer is installed. A diagram showing the connection of such a system is provided below.

Choosing the right capacitor or voltage stabilizer is extremely important if we care about proper ripple suppression and voltage stabilization. The selection of this second element is made taking into account such input parameters as nominal power, the speed of voltage changes, or the voltage range at the input. If, on the other hand, we are talking about a capacitor filtering the signal after exiting the Graetz bridge, it should be calculated based on the mathematical dependencies presented below.

The input data we need to know before starting the calculations are:

  • Supply voltage UZ [V];
  • Current consumption value I [A];
  • Period for the given rectifier that will be used in the system t [ms].

Having knowledge of the desired ripple amplitude level (specific to the sensitivity of the powered device), we can calculate the voltage value U.

If we assume that the maximum allowable ripple amplitude value will be 7% for a given application, and the supply UZ=24V, then the calculated voltage U=0.07*24=1.68V.

Next, let's assume that the period for our rectifier takes the value t=12ms, and the current consumption is 0.6A. The minimum capacitance of the capacitor that should be selected for such a rectifier bridge system is:

Having this value, we can use this parameter in the TME catalog and we can very efficiently select the appropriate type of capacitor for the rectifier bridge system.

Practical application of rectifier bridges

Rectifier bridges are an essential element of the power supply system for a stepper motor or servo motor based on direct current. No household appliance that requires direct current for its operation can do without them. A power supply equipped with a high-quality Graetz bridge, supported by a voltage stabilizer and a filter in the form of a capacitor will be a safe and effective solution when it comes to delivering electrical energy to a smartphone, tablet, TV, or laptop.

How can you assess whether a rectifier bridge is operational?

To ensure that the Graetz bridge is working correctly, it is enough to use the simplest electrical meter – a multimeter. It will allow measuring each of the four diodes, which will clearly determine the rectifier bridge's ability to continue working. When selecting the appropriate specimen for your application, it is worth keeping in mind that the quality of workmanship and the materials used determine how our device will be powered. Considering that currently very complex and expensive systems contained in our electronics are extremely susceptible to all types of power anomalies, it is not worth experimenting with untested electronic components. The TME catalog offers a range of the highest quality rectifier bridges from proven electronics manufacturers. Such a choice will certainly ensure that the product's lifespan will be satisfactory and will not require additional diagnostics or financial outlays.

How to check a rectifier bridge with a multimeter

If indeed a situation arises where we are forced to examine our rectifier bridge, the ability to operate a multimeter will be essential. To measure the individual diodes, the following sequence should be performed: the black test lead connected to the COM socket in the multimeter is connected to the positive connector, while the red test lead is connected to the direct current diode connector. If we want to measure using the negative alternating current terminal, then we connect the red test lead to it, and the black lead closes the meter circuit on the measured diode. The expected results in both cases should be values close to zero. This indicates the good condition of the measured diodes.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.