+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Free vibrations are a type of oscillatory motion of a mechanical, electrical, or other dynamic system that, after an initial displacement from the equilibrium position, oscillates without further action of external forces. This motion results from the internal forces of the system, such as the force of elasticity, the force of inertia, and, in the presence of resistance, the force of damping. Free vibrations occur in many physical systems, ranging from simple mass-spring models to complex electromechanical systems and building structures.
The frequency of free vibrations, known as the natural frequency, depends solely on the physical properties of the system, such as mass, stiffness, and damping characteristics. In systems with negligible damping, these vibrations can last for a long time, whereas in heavily damped systems, the amplitude of the vibrations quickly decreases due to energy dissipation in the form of heat or other energy losses.
The mathematical description of free vibrations is based on second-order differential equations, whose solutions indicate that the system's response can be in the form of damped harmonic oscillations or, in the case of strong damping, a non-oscillatory response. In engineering and mechanics, free vibrations are analyzed to determine the resistance of structures to vibrations, assess the stability of dynamic systems, and design devices with specified dynamic characteristics.
In many technical fields, such as construction, automotive, aviation, and materials engineering, controlling free vibrations is crucial for ensuring the durability, comfort of use, and operational safety of technical systems. The phenomenon of resonance, which occurs when the frequency of external excitation matches the natural frequency of the system, is directly related to the analysis of free vibrations and is a significant element in the engineering design process.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.