+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
A Bridge Rectifier is an electronic circuit used to convert alternating voltage (AC) to direct voltage (DC) by exploiting the properties of non-linear semiconductor elements. Its operating principle is based on double-voltage rectification, which means that both the positive and negative halves of the input voltage waveform are converted into unidirectional current flow, eliminating the pause periods characteristic of single-voltage rectification systems.
Bridge rectifiers' structure consists of four diodes connected in a Graetz configuration, which ensures efficient rectification of the input voltage while maintaining high energy efficiency. In the conduction phase, the Diodes are controlled by the input voltage, allowing current to flow in one direction regardless of the polarity of the input signal, while in the blocking phase they prevent reversal of the polarity of the output voltage.
Bridge rectifiers' electrical characteristics depend on the parameters of the diodes used, such as threshold voltage, conduction current and heat dissipation capability. High-current circuits use bridges equipped with Heatsinks or additional cooling layers to reduce component heating and minimise power losses due to the Joule effect. Bridge rectifiers can be made using silicon (Si) diode technology or modern structures based on silicon carbide (SiC) and gallium nitride (GaN), which have lower switching losses and higher resistance to overvoltage.
In power systems, Bridge rectifiers work with capacitive and inductive filters to reduce output voltage ripple, improving stability and DC signal quality. In applications requiring precise control of the output voltage, compensating circuits and pulse regulators are used to correct the characteristics of the rectified voltage according to the requirements of the receiving system.
Bridge rectifiers are used in a wide range of electrical and electronic devices including switching power supplies, battery charging systems, electric motor drive systems and energy converters used in renewable energy sources. In industrial designs, bridges can be part of complex power electronic systems where they work in conjunction with Thyristors or power transistors to enable controlled voltage rectification with simultaneous regulation of rms current and output voltage.
Optimisation of bridge rectifiers topologies includes the use of Schottky diodes in low-voltage circuits to reduce conduction losses, and the implementation of active rectification technology using digitally controlled MOSFETs that eliminate the voltage drops inherent in traditional semiconductor diodes, thereby increasing the energy efficiency of power conversion systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.