+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Multiplexer (MUX) - definition

Multiplexer (MUX) is a digital or analogue circuit used to select one signal from multiple inputs and transmit it to a common output, depending on the logic state of the control lines. It acts as a selector, allowing data from different sources to be transmitted over a single transmission medium, making efficient use of system resources and simplifying electronic circuit architecture.

In digital electronics, multiplexers are used as logic elements in control systems, data switching and the implementation of logical and arithmetic functions. They operate by decoding a control signal that indicates which input will be connected to the output. In practice, the number of inputs is a power of two and the number of address lines determines how many bits are needed to select a particular channel.

In transmission systems multiplexing allows multiple signals to be transmitted over a single communication channel by separating them in the time, frequency, wavelength or code domains. This approach is used in telecommunications, data transmission, fibre optic systems and Computer Networks, among others. In this form, the multiplexer acts as a device that aggregates signals and allows them to be transmitted together and subsequently separated in a demultiplexer.

The construction and implementation of a multiplexer can be realised using logic gates, Programmable circuits (e.g. FPGAs) or as off-the-shelf integrated components. Depending on the intended use, the circuit can be adapted to work with binary, analogue or mixed signals. Multiplexers are the foundation of many digital and Automation systems, where flexible and dynamic control of information flow is required.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO