+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
PAM (Pulse-Amplitude Modulation) is a pulse modulation technique in which information is encoded by changing the amplitude of successive pulses over time. Each pulse carries a specific value of an analogue or digital signal, representing the voltage level corresponding to a sample of the modulating signal. The time of occurrence of the pulses and their width remain constant, while only their height changes, according to the current value of the input signal.
PAM modulation is one of the basic forms of modulation in data transmission and analogue-to-digital conversion systems. In digital applications, pulse amplitudes take on values from a fixed set of discrete levels, allowing each value to be assigned a binary code. In analogue, the amplitude changes continuously, mapping the original signal waveform.
Others use the technique in various areas of telecommunications and electronics, including data transmission over wired channels, next-generation Ethernet systems (e.g. 100GBASE-PAM4), analogue-to-digital converters and optical communications. Due to its simplicity, PAM is often used as a basic stage in more complex modulation schemes such as QAM (Quadrature Amplitude Modulation).
One important aspect of PAM is its susceptibility to linear and non-linear noise and distortion, which requires advanced error correction and filtering methods. In addition, increasing the number of digital amplitude levels (e.g. PAM-4, PAM-8) allows more data to be transmitted in the same bandwidth, but at the same time increases sensitivity to noise and detection errors. Therefore, the design of systems using PAM requires precise adjustment of the transmission path parameters and the use of appropriate modulation and demodulation algorithms.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.