+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Tabulation - definition

Tabulating (lookup table, LUT) is a technique used in computer science, electronics and digital systems to replace complex calculations or logic operations by direct access to pre-prepared results stored in an array. Instead of recalculating the value of a function each time in real time, the system refers to a ready-made set of data, which significantly reduces processing time and reduces the hardware or software complexity of the solution.

LUTs are commonly used in microprocessors, FPGAs, DSP (Digital Signal Processing) systems, as well as in computer graphics algorithms, data compression or encoding. In digital circuits, the LUT often has the function of mapping input bits to specific output states according to predefined logic. In the context of programming, arrays allow e.g. fast calculation of values of trigonometric functions, logarithms or interpolation operations, which is particularly important in systems with limited computing resources.

In digital electronics, especially in programmable logic structures such as FPGAs, LUTs are the basic blocks that implement combinational functions. Each LUT can map any binary logic function depending on the number of inputs, making it a versatile and flexible tool for implementing user logic. In this case, arrays contribute to shortening the logic paths and thus improving the speed of the entire circuit.

Arraying can be implemented in both static memory (ROM, SRAM) and dynamic memory, and its effectiveness depends on the proper design of the addressing structure and the way the data is stored. It is an effective method especially when the calculation of function values is time or resource intensive and the number of possible inputs is limited and well defined.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO