+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

IR LEDs

(694)

IR LEDs (infrared) are a popular solution in at least two areas: lightning for monitoring systems and wireless communication. They are available in formats that are similar to elements emitting visible light and are characterized by similar electric parameters. Low price and easy mounting are just two indisputable assets.

IR as a method of lightning

Infrared radiation, also called IR, is electromagnetic radiation with the wavelength from to 1mm up to 700nm. As such frequencies are invisible to the human eye and at the same time safe for health, they are used in wireless communication systems, sensors, and many other devices as well as in research methods**.

For example, radiation with the wavelength from 840nm up to 960nm is used as lighting recorded only by special cameras. These devices make it possible to conduct observation in (apparent) darkness, e.g. in monitoring systems (CCTV) or camera traps(maintenance-free cameras triggered by motion sensors). Thanks to the “invisibility” of infrared radiation, it can be used in many alarm systems. In the automotive sector, miniature sources of infrared radiation are used as non-invasive ICMS lightning (in-cabin monitoring system). Thanks to them, the on-board computer analyses the driver’s behaviour even at night: in case of danger (when the driver falls unconscious) ICMS automatically sets the alarm on and gradually brings the car to a full stop. In this area, IR LEDs are also used to illuminate the surroundings for sensors monitoring traffic around the car. Another related application are interfaces recognizing user’s gestures – they are also based on registering image in the spectrum of infrared radiation.

Chart_visible_light

Fig. 1. Visible light, recorded by CCD and emitted by LEDs IRIncluded values.

Chart (Fig. 1) illustrates the comparison of averaged and included values for the following spectrum variants: human eye responsiveness (red line); responsivity of a typical CCD used in CCTV (blue line); the emission of infrared light by sample IR LEDs – yellow line (840-870nm models), purple line (920-960nm models).

Infrared radiation in wireless communication

Diodes emitting infrared radiation are used in wireless data transmission. A typical application are remote TV controls. However, many products available from TME are characterized by power that is higher than required by a typical TV remote control.

Transmission of data using infrared radiation signals is used in production plants whereit is applied in M2M communication (machine-to-machine). Another area where high power IR LEDs serve as transmitters are panels used for wireless transmission of sound (in digital form). They are often installed in lecture halls, cinemas, and theatres, where they transmit the signal from interpreters to receivers/headsets during international conferences, film, theatre, and opera festivals, etc. Although this transmission method has lost some of its popularity in the last decade, its great advantage is easy implementation (temporary installations) as well as immunity to EMC that may be caused by mobile phones and stage equipment.

Most of microcontroller platforms (AVR, PIC, Arduino etc.) and single-board systems have open source libraries enabling the transmission of instructions using standard protocols of transmission in infrared radiation (SIRC, RC5, RC5, etc.) From the technical point of view, connecting IR LEDs to control circuit e.g. via a microcontroller is not problematic because a standard transistor can function as a driver. Of course, it is a simplified example – in most cases a specially designed system enabling to control the emission with high frequency would be the best solution.

It needs to be taken into account that communication with the use of infrared radiation is often impossible (or significantly limited) in sunny spots.

Crucial parameters of IR LEDs

In the specification of products from this category, you can find a range of values typical for LEDs – power, maximum current, operating voltage, mounting method. Infrared elements (especially when used as a form of lighting) are often installed on matrices – this means that SMD packages are a popular variant.

Depending on the device, a demand for a space lit by infrared radiation will be different. In order to send signals controlling or observing the driver via ICMS, a narrow angle of emission is required, while the illumination for monitoring should cover the whole area observed by the camera. This is whyLEDs are characterized by a viewing angle from od 3° do 160° – this value is usually listed among basic parameters of each element.

The wavelength of emitted radiation may occur extremely crucial. In the case of lightning it has to be in accordance with the characteristics of the sensor used, whereas in devices for communication you have to remember about the compatibility between the transmitting and receiving elements. IR receivers are characterized by selectivity – thanks to this, they are immune to interference (sources of visible light). This means that an IR LED has to be adjusted so that its radiation is recorded by the optoelectrical element. Eventually, for many applications the LED optic power is a key factor. The reach of transmission as well as the intensity of illumination are dependent on it. At TME, you can find IR LEDs with the power starting from 0.2mW (used in energy-saving sensors) to products whose power exceeds 1W (elements typical for CCTV used at night).

Products: 694

Warehouse:

TME
External
All
Page 1
TSAL6200 | IR transmitter; 5mm; 940nm; blue-grey,transparent; 210mW; 17°; THT
IR transmitter; 5mm; 940nm; blue-grey,transparent; 210mW; 17°; THT
Manufacturer part number: TSAL6200
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.41 USDGross price for quantities from 1 pcs - 0.41 USD
Net price for quantities from 10 pcs - 0.31 USDGross price for quantities from 10 pcs - 0.31 USD
Net price for quantities from 50 pcs - 0.22 USDGross price for quantities from 50 pcs - 0.22 USD
Net price for quantities from 60 pcs - 0.21 USDGross price for quantities from 60 pcs - 0.21 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 300 pcs - 0.15 USDGross price for quantities from 300 pcs - 0.15 USD
Net price for quantities from 500 pcs - 0.14 USDGross price for quantities from 500 pcs - 0.14 USD
Net price for quantities from 1000 pcs - 0.13 USDGross price for quantities from 1000 pcs - 0.13 USD
12968 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SFH 4550 | IR transmitter; 5mm; 860nm; transparent; 1100mW; 3°; 1.5÷2.4VDC
IR transmitter; 5mm; 860nm; transparent; 1100mW; 3°; 1.5÷2.4VDC
Manufacturer part number: SFH 4550
Manufacturer: ams OSRAM
Net price for quantities from 1 pcs - 0.87 USDGross price for quantities from 1 pcs - 0.87 USD
Net price for quantities from 10 pcs - 0.54 USDGross price for quantities from 10 pcs - 0.54 USD
Net price for quantities from 25 pcs - 0.43 USDGross price for quantities from 25 pcs - 0.43 USD
Net price for quantities from 50 pcs - 0.37 USDGross price for quantities from 50 pcs - 0.37 USD
Net price for quantities from 100 pcs - 0.33 USDGross price for quantities from 100 pcs - 0.33 USD
Net price for quantities from 250 pcs - 0.29 USDGross price for quantities from 250 pcs - 0.29 USD
Net price for quantities from 300 pcs - 0.29 USDGross price for quantities from 300 pcs - 0.29 USD
Net price for quantities from 500 pcs - 0.28 USDGross price for quantities from 500 pcs - 0.28 USD
Net price for quantities from 1000 pcs - 0.27 USDGross price for quantities from 1000 pcs - 0.27 USD
11200 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LIR30243-01 | IR transmitter; 3mm; 940nm; transparent; 25°; THT; 20mA
IR transmitter; 3mm; 940nm; transparent; 25°; THT; 20mA
Manufacturer part number: LIR30243-01
Manufacturer: WENRUN
Net price for quantities from 5 pcs - 0.13 USDGross price for quantities from 5 pcs - 0.13 USD
Net price for quantities from 30 pcs - 0.08 USDGross price for quantities from 30 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.05 USDGross price for quantities from 100 pcs - 0.05 USD
Net price for quantities from 500 pcs - 0.04 USDGross price for quantities from 500 pcs - 0.04 USD
Net price for quantities from 2000 pcs - 0.03 USDGross price for quantities from 2000 pcs - 0.03 USD
24142 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 5.
Multiplicity: 1.
L-934F3C | IR transmitter; 3mm; 940nm; transparent; 3.6mW; 30°; THT
IR transmitter; 3mm; 940nm; transparent; 3.6mW; 30°; THT
Manufacturer part number: L-934F3C
Manufacturer: KINGBRIGHT ELECTRONIC
Net price for quantities from 1 pcs - 0.18 USDGross price for quantities from 1 pcs - 0.18 USD
Net price for quantities from 5 pcs - 0.15 USDGross price for quantities from 5 pcs - 0.15 USD
Net price for quantities from 1000 pcs - 0.14 USDGross price for quantities from 1000 pcs - 0.14 USD
21893 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
L-934F3BT | IR transmitter; 3mm; 940nm; blue,transparent; 3.6mW; 50°; THT
IR transmitter; 3mm; 940nm; blue,transparent; 3.6mW; 50°; THT
Manufacturer part number: L-934F3BT
Manufacturer: KINGBRIGHT ELECTRONIC
Net price for quantities from 1 pcs - 0.18 USDGross price for quantities from 1 pcs - 0.18 USD
Net price for quantities from 10 pcs - 0.15 USDGross price for quantities from 10 pcs - 0.15 USD
Net price for quantities from 75 pcs - 0.13 USDGross price for quantities from 75 pcs - 0.13 USD
Net price for quantities from 150 pcs - 0.13 USDGross price for quantities from 150 pcs - 0.13 USD
Net price for quantities from 300 pcs - 0.12 USDGross price for quantities from 300 pcs - 0.12 USD
Net price for quantities from 500 pcs - 0.12 USDGross price for quantities from 500 pcs - 0.12 USD
Net price for quantities from 600 pcs - 0.12 USDGross price for quantities from 600 pcs - 0.12 USD
Net price for quantities from 1000 pcs - 0.11 USDGross price for quantities from 1000 pcs - 0.11 USD
Net price for quantities from 2000 pcs - 0.11 USDGross price for quantities from 2000 pcs - 0.11 USD
Net price for quantities from 4000 pcs - 0.11 USDGross price for quantities from 4000 pcs - 0.11 USD
15961 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SFH 4356 | IR transmitter; 3mm; 860nm; black; 90mW; 20°; 1.7÷2VDC; THT; 100mA
IR transmitter; 3mm; 860nm; black; 90mW; 20°; 1.7÷2VDC; THT; 100mA
Manufacturer part number: SFH 4356
Manufacturer: ams OSRAM
Net price for quantities from 1 pcs - 0.51 USDGross price for quantities from 1 pcs - 0.51 USD
Net price for quantities from 10 pcs - 0.38 USDGross price for quantities from 10 pcs - 0.38 USD
Net price for quantities from 25 pcs - 0.31 USDGross price for quantities from 25 pcs - 0.31 USD
Net price for quantities from 50 pcs - 0.27 USDGross price for quantities from 50 pcs - 0.27 USD
Net price for quantities from 100 pcs - 0.23 USDGross price for quantities from 100 pcs - 0.23 USD
Net price for quantities from 300 pcs - 0.20 USDGross price for quantities from 300 pcs - 0.20 USD
Net price for quantities from 400 pcs - 0.20 USDGross price for quantities from 400 pcs - 0.20 USD
Net price for quantities from 500 pcs - 0.20 USDGross price for quantities from 500 pcs - 0.20 USD
Net price for quantities from 2000 pcs - 0.18 USDGross price for quantities from 2000 pcs - 0.18 USD
12194 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
TSAL6400 | IR transmitter; 5mm; 940nm; blue,transparent; 160mW; 25°; THT
IR transmitter; 5mm; 940nm; blue,transparent; 160mW; 25°; THT
Manufacturer part number: TSAL6400
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.44 USDGross price for quantities from 1 pcs - 0.44 USD
Net price for quantities from 10 pcs - 0.33 USDGross price for quantities from 10 pcs - 0.33 USD
Net price for quantities from 50 pcs - 0.24 USDGross price for quantities from 50 pcs - 0.24 USD
Net price for quantities from 100 pcs - 0.20 USDGross price for quantities from 100 pcs - 0.20 USD
Net price for quantities from 300 pcs - 0.16 USDGross price for quantities from 300 pcs - 0.16 USD
Net price for quantities from 500 pcs - 0.14 USDGross price for quantities from 500 pcs - 0.14 USD
Net price for quantities from 1000 pcs - 0.14 USDGross price for quantities from 1000 pcs - 0.14 USD
1463 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
HSDL-4230 | IR transmitter; 5mm; 860÷895nm,875nm; transparent; 75mW; 17°; THT
IR transmitter; 5mm; 860÷895nm,875nm; transparent; 75mW; 17°; THT
Manufacturer part number: HSDL-4230
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.89 USDGross price for quantities from 1 pcs - 0.89 USD
Net price for quantities from 10 pcs - 0.39 USDGross price for quantities from 10 pcs - 0.39 USD
Net price for quantities from 100 pcs - 0.25 USDGross price for quantities from 100 pcs - 0.25 USD
Net price for quantities from 250 pcs - 0.24 USDGross price for quantities from 250 pcs - 0.24 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1000 pcs - 0.22 USDGross price for quantities from 1000 pcs - 0.22 USD
Net price for quantities from 2000 pcs - 0.21 USDGross price for quantities from 2000 pcs - 0.21 USD
Net price for quantities from 5000 pcs - 0.21 USDGross price for quantities from 5000 pcs - 0.21 USD
15306 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SFH 4350 | IR transmitter; 3mm; 860nm; transparent; 200mW; 13°; 1.5÷1.8VDC
IR transmitter; 3mm; 860nm; transparent; 200mW; 13°; 1.5÷1.8VDC
Manufacturer part number: SFH 4350
Manufacturer: ams OSRAM
Net price for quantities from 1 pcs - 0.92 USDGross price for quantities from 1 pcs - 0.92 USD
Net price for quantities from 10 pcs - 0.69 USDGross price for quantities from 10 pcs - 0.69 USD
Net price for quantities from 25 pcs - 0.60 USDGross price for quantities from 25 pcs - 0.60 USD
Net price for quantities from 30 pcs - 0.58 USDGross price for quantities from 30 pcs - 0.58 USD
Net price for quantities from 50 pcs - 0.54 USDGross price for quantities from 50 pcs - 0.54 USD
Net price for quantities from 100 pcs - 0.48 USDGross price for quantities from 100 pcs - 0.48 USD
Net price for quantities from 250 pcs - 0.41 USDGross price for quantities from 250 pcs - 0.41 USD
Net price for quantities from 500 pcs - 0.36 USDGross price for quantities from 500 pcs - 0.36 USD
Net price for quantities from 1000 pcs - 0.32 USDGross price for quantities from 1000 pcs - 0.32 USD
Net price for quantities from 2000 pcs - 0.31 USDGross price for quantities from 2000 pcs - 0.31 USD
11477 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LL-304IRC4B-2AD | IR transmitter; 3mm; 940nm; transparent; 30°; THT; 100mW; 6÷10mW/sr
IR transmitter; 3mm; 940nm; transparent; 30°; THT; 100mW; 6÷10mW/sr
Manufacturer part number: LL-304IRC4B-2AD
Manufacturer: LUCKYLIGHT
Net price for quantities from 5 pcs - 0.13 USDGross price for quantities from 5 pcs - 0.13 USD
Net price for quantities from 25 pcs - 0.07 USDGross price for quantities from 25 pcs - 0.07 USD
Net price for quantities from 100 pcs - 0.05 USDGross price for quantities from 100 pcs - 0.05 USD
Net price for quantities from 500 pcs - 0.04 USDGross price for quantities from 500 pcs - 0.04 USD
Net price for quantities from 2000 pcs - 0.04 USDGross price for quantities from 2000 pcs - 0.04 USD
16472 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 5.
Multiplicity: 1.
IR15-21C/TR8 | IR transmitter; 940nm; transparent; 160°; 1.2÷1.5VDC; SMD; 65mA
IR transmitter; 940nm; transparent; 160°; 1.2÷1.5VDC; SMD; 65mA
Manufacturer part number: IR15-21C/TR8
Manufacturer: EVERLIGHT
Net price for quantities from 1 pcs - 0.15 USDGross price for quantities from 1 pcs - 0.15 USD
Net price for quantities from 10 pcs - 0.10 USDGross price for quantities from 10 pcs - 0.10 USD
Net price for quantities from 50 pcs - 0.08 USDGross price for quantities from 50 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.08 USDGross price for quantities from 100 pcs - 0.08 USD
Net price for quantities from 250 pcs - 0.08 USDGross price for quantities from 250 pcs - 0.08 USD
19432 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
Product available till the stock lasts
LTE-302 | IR transmitter; 940nm; transparent; 0.662÷2.165mW; 40°; THT; 20mA
IR transmitter; 940nm; transparent; 0.662÷2.165mW; 40°; THT; 20mA
Manufacturer part number: LTE-302
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.35 USDGross price for quantities from 1 pcs - 0.35 USD
Net price for quantities from 10 pcs - 0.27 USDGross price for quantities from 10 pcs - 0.27 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.14 USDGross price for quantities from 500 pcs - 0.14 USD
Net price for quantities from 1000 pcs - 0.12 USDGross price for quantities from 1000 pcs - 0.12 USD
Net price for quantities from 2000 pcs - 0.11 USDGross price for quantities from 2000 pcs - 0.11 USD
Net price for quantities from 5000 pcs - 0.09 USDGross price for quantities from 5000 pcs - 0.09 USD
Net price for quantities from 10000 pcs - 0.08 USDGross price for quantities from 10000 pcs - 0.08 USD
Net price for quantities from 20000 pcs - 0.07 USDGross price for quantities from 20000 pcs - 0.07 USD
Net price for quantities from 25000 pcs - 0.07 USDGross price for quantities from 25000 pcs - 0.07 USD
9806 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
TSAL6100 | IR transmitter; 5mm; 940nm; blue-grey,transparent; 40mW; THT
IR transmitter; 5mm; 940nm; blue-grey,transparent; 40mW; THT
Manufacturer part number: TSAL6100
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.66 USDGross price for quantities from 1 pcs - 0.66 USD
Net price for quantities from 10 pcs - 0.40 USDGross price for quantities from 10 pcs - 0.40 USD
Net price for quantities from 25 pcs - 0.34 USDGross price for quantities from 25 pcs - 0.34 USD
Net price for quantities from 50 pcs - 0.29 USDGross price for quantities from 50 pcs - 0.29 USD
Net price for quantities from 100 pcs - 0.25 USDGross price for quantities from 100 pcs - 0.25 USD
Net price for quantities from 500 pcs - 0.15 USDGross price for quantities from 500 pcs - 0.15 USD
Net price for quantities from 1000 pcs - 0.14 USDGross price for quantities from 1000 pcs - 0.14 USD
Net price for quantities from 2000 pcs - 0.13 USDGross price for quantities from 2000 pcs - 0.13 USD
Net price for quantities from 4000 pcs - 0.13 USDGross price for quantities from 4000 pcs - 0.13 USD
Net price for quantities from 8000 pcs - 0.12 USDGross price for quantities from 8000 pcs - 0.12 USD
4225 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
VSLB3940 | IR transmitter; 3mm; 940nm; transparent; 40mW; 44°; 1.15÷1.6VDC
IR transmitter; 3mm; 940nm; transparent; 40mW; 44°; 1.15÷1.6VDC
Manufacturer part number: VSLB3940
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.61 USDGross price for quantities from 1 pcs - 0.61 USD
Net price for quantities from 5 pcs - 0.53 USDGross price for quantities from 5 pcs - 0.53 USD
Net price for quantities from 10 pcs - 0.48 USDGross price for quantities from 10 pcs - 0.48 USD
Net price for quantities from 20 pcs - 0.43 USDGross price for quantities from 20 pcs - 0.43 USD
Net price for quantities from 100 pcs - 0.31 USDGross price for quantities from 100 pcs - 0.31 USD
Net price for quantities from 200 pcs - 0.28 USDGross price for quantities from 200 pcs - 0.28 USD
Net price for quantities from 500 pcs - 0.24 USDGross price for quantities from 500 pcs - 0.24 USD
Net price for quantities from 1000 pcs - 0.22 USDGross price for quantities from 1000 pcs - 0.22 USD
Net price for quantities from 5000 pcs - 0.18 USDGross price for quantities from 5000 pcs - 0.18 USD
Net price for quantities from 10000 pcs - 0.16 USDGross price for quantities from 10000 pcs - 0.16 USD
12032 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
TSAL4400 | IR transmitter; 3mm; 940nm; transparent,grey; 160mW; 25°; THT
IR transmitter; 3mm; 940nm; transparent,grey; 160mW; 25°; THT
Manufacturer part number: TSAL4400
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.44 USDGross price for quantities from 1 pcs - 0.44 USD
Net price for quantities from 5 pcs - 0.35 USDGross price for quantities from 5 pcs - 0.35 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 25 pcs - 0.23 USDGross price for quantities from 25 pcs - 0.23 USD
Net price for quantities from 100 pcs - 0.16 USDGross price for quantities from 100 pcs - 0.16 USD
Net price for quantities from 250 pcs - 0.13 USDGross price for quantities from 250 pcs - 0.13 USD
Net price for quantities from 300 pcs - 0.12 USDGross price for quantities from 300 pcs - 0.12 USD
Net price for quantities from 500 pcs - 0.12 USDGross price for quantities from 500 pcs - 0.12 USD
4107 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
TSHF5210 | IR transmitter; 5mm; 890nm; transparent; 180mW; 10°; THT
IR transmitter; 5mm; 890nm; transparent; 180mW; 10°; THT
Manufacturer part number: TSHF5210
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.65 USDGross price for quantities from 1 pcs - 0.65 USD
Net price for quantities from 10 pcs - 0.47 USDGross price for quantities from 10 pcs - 0.47 USD
Net price for quantities from 25 pcs - 0.40 USDGross price for quantities from 25 pcs - 0.40 USD
Net price for quantities from 50 pcs - 0.35 USDGross price for quantities from 50 pcs - 0.35 USD
Net price for quantities from 100 pcs - 0.30 USDGross price for quantities from 100 pcs - 0.30 USD
Net price for quantities from 500 pcs - 0.21 USDGross price for quantities from 500 pcs - 0.21 USD
Net price for quantities from 1000 pcs - 0.20 USDGross price for quantities from 1000 pcs - 0.20 USD
714 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LL-503IRT2E-2AC | IR transmitter; 5mm; 940nm; blue,transparent; 20°; THT; 100mW
IR transmitter; 5mm; 940nm; blue,transparent; 20°; THT; 100mW
Manufacturer part number: LL-503IRT2E-2AC
Manufacturer: LUCKYLIGHT
Net price for quantities from 5 pcs - 0.12 USDGross price for quantities from 5 pcs - 0.12 USD
Net price for quantities from 25 pcs - 0.07 USDGross price for quantities from 25 pcs - 0.07 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 500 pcs - 0.05 USDGross price for quantities from 500 pcs - 0.05 USD
Net price for quantities from 2000 pcs - 0.04 USDGross price for quantities from 2000 pcs - 0.04 USD
9935 in TME stock
No. of pieces (Multiplicity: 5)
Minimum order quantity: 5.
Multiplicity: 5.
L-53F3C | IR transmitter; 5mm; 940nm; transparent; 20mW; 30°; THT
IR transmitter; 5mm; 940nm; transparent; 20mW; 30°; THT
Manufacturer part number: L-53F3C
Manufacturer: KINGBRIGHT ELECTRONIC
Net price for quantities from 1 pcs - 0.23 USDGross price for quantities from 1 pcs - 0.23 USD
Net price for quantities from 10 pcs - 0.17 USDGross price for quantities from 10 pcs - 0.17 USD
Net price for quantities from 50 pcs - 0.15 USDGross price for quantities from 50 pcs - 0.15 USD
Net price for quantities from 100 pcs - 0.15 USDGross price for quantities from 100 pcs - 0.15 USD
Net price for quantities from 250 pcs - 0.14 USDGross price for quantities from 250 pcs - 0.14 USD
Net price for quantities from 500 pcs - 0.14 USDGross price for quantities from 500 pcs - 0.14 USD
Net price for quantities from 1000 pcs - 0.13 USDGross price for quantities from 1000 pcs - 0.13 USD
Net price for quantities from 2000 pcs - 0.13 USDGross price for quantities from 2000 pcs - 0.13 USD
Net price for quantities from 5000 pcs - 0.12 USDGross price for quantities from 5000 pcs - 0.12 USD
5102 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LTE-3371T | IR transmitter; 5mm; 940nm; transparent; 40°; 1.25÷1.6VDC; THT
IR transmitter; 5mm; 940nm; transparent; 40°; 1.25÷1.6VDC; THT
Manufacturer part number: LTE-3371T
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.35 USDGross price for quantities from 1 pcs - 0.35 USD
Net price for quantities from 10 pcs - 0.25 USDGross price for quantities from 10 pcs - 0.25 USD
Net price for quantities from 100 pcs - 0.17 USDGross price for quantities from 100 pcs - 0.17 USD
Net price for quantities from 500 pcs - 0.14 USDGross price for quantities from 500 pcs - 0.14 USD
Net price for quantities from 1000 pcs - 0.14 USDGross price for quantities from 1000 pcs - 0.14 USD
Net price for quantities from 5000 pcs - 0.13 USDGross price for quantities from 5000 pcs - 0.13 USD
14692 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SFH 4554 | IR transmitter; 5mm; 860nm; black; 550mW; 10°; 1.7÷3.6VDC; THT
IR transmitter; 5mm; 860nm; black; 550mW; 10°; 1.7÷3.6VDC; THT
Manufacturer part number: SFH 4554
Manufacturer: ams OSRAM
Net price for quantities from 1 pcs - 0.75 USDGross price for quantities from 1 pcs - 0.75 USD
Net price for quantities from 10 pcs - 0.50 USDGross price for quantities from 10 pcs - 0.50 USD
Net price for quantities from 25 pcs - 0.36 USDGross price for quantities from 25 pcs - 0.36 USD
Net price for quantities from 50 pcs - 0.29 USDGross price for quantities from 50 pcs - 0.29 USD
Net price for quantities from 100 pcs - 0.24 USDGross price for quantities from 100 pcs - 0.24 USD
Net price for quantities from 125 pcs - 0.24 USDGross price for quantities from 125 pcs - 0.24 USD
Net price for quantities from 1000 pcs - 0.22 USDGross price for quantities from 1000 pcs - 0.22 USD
3857 in TME stock