+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The farad (F) is the SI unit of electrical capacitance, defined as the capacity to store one coulomb (C) of electric charge when subjected to a potential difference of one volt (V). The unit is named after Michael Faraday, a British physicist and chemist who made pioneering contributions to the development of electromagnetism and electrochemistry. Capacitance describes a system’s ability to store energy in an electrostatic field, and the farad is the standard unit used to quantify this property.
In practical terms, the farad is a very large unit, so its submultiples—such as the microfarad (μF), nanofarad (nF), and picofarad (pF)—are more commonly used in technical applications. The primary component that exhibits capacitance is the capacitor, a device consisting of two conductive plates separated by a dielectric material. The amount of charge a capacitor can store depends on the applied voltage and the type and geometry of the dielectric used. The greater the capacitance, the more energy the capacitor can store at a given voltage.
In electronic circuits, capacitance measured in farads influences the circuit’s temporal behavior, such as delay, signal attenuation, or filtering capability. Capacitors of various capacitances are used in power supplies, resonant circuits, filters, converters, and timing circuits. Capacitance also plays an essential role in energy transmission, charge storage, and the design of microwave components and integrated electronic structures.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.