+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Direct current (DC) is a form of electric charge flow in which the direction and magnitude of the current remain constant over time. It is characterized by a uniform movement of electrons from a point of higher electric potential to a point of lower potential, resulting in a continuous unidirectional current. This method of electrical energy conduction enables stable power supply to electronic circuits and precise control of components sensitive to voltage fluctuations.
Sources of direct current include galvanic cells, batteries, switch-mode power supplies, and voltage converters that transform alternating current into direct current. Technologically, DC is used wherever reliability, precision, or low electromagnetic interference is required—from digital systems and automation equipment to brushed and brushless motor drives.
In electrical circuit analysis, direct current allows for simplified mathematical modeling, as its parameters are time-independent. This enables the straightforward application of Ohm’s law and energy conservation principles without the need for dynamic analysis. Unlike alternating current, DC does not involve phenomena such as reactance or phase shift, which simplifies the design and analysis of many power systems and devices.
Direct current plays an increasingly important role in power systems, particularly in the context of renewable energy development, energy storage, and long-distance high-voltage transmission (HVDC). Its use contributes to improved energy efficiency and facilitates the integration of diverse energy sources and loads within smart power grids. However, it also requires dedicated protection and conversion systems, adapted to the specific nature of unidirectional charge flow and the need for stable operating voltage.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.