+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Rectifier is an electrical or electronic circuit used to convert alternating current (AC) into direct current (DC), primarily utilized in power supply systems for electronic devices as well as in the power industry and automation. Its operation is based on the use of nonlinear components, most commonly semiconductor diodes, which conduct current in only one direction while blocking it in the opposite direction. This allows the elimination of the negative half-cycles of a sinusoidal waveform and enables unidirectional current flow.
In its simplest form, a rectifier converts AC voltage into a pulsating DC current, which can then be smoothed using additional components such as capacitors or inductors. In more advanced configurations, such as multiphase rectifier circuits or bridge rectifiers (Graetz bridges), higher efficiency, lower voltage ripple, and compatibility with various input voltage configurations are achieved. Modern systems also employ controlled rectifiers using thyristors or transistors, allowing for regulation of the output voltage and integration with automation systems.
Rectifiers play a crucial role in switch-mode power supplies, battery chargers, frequency converters, uninterruptible power supplies (UPS), traction systems, DC motor drives, and renewable energy conversion systems. Their design and technical specifications must consider not only conversion efficiency but also overload resistance, electromagnetic interference, harmonic emissions, and compliance with safety standards. The effective operation of a rectifier directly impacts the stability and quality of power supply, which is particularly important in systems sensitive to voltage and current disturbances.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.