Car Speakers

(893)

One of the most common modifications drivers are making, is the replacement or modification of car audio systems . The reason for this could be an unsatisfactory HiFi system installed by the car manufacturer, the lack of a sound system (less commonly), or simply wear and tear. Due to working in harsh conditions (vibrations, shocks) , car speakers are susceptible to mechanical damage.

Car speakers include several product groups that serve to improve the acoustic performance and sound quality in the car. These include the basic components of a car audio system, as well as mounting accessories. These products are dedicated to both car enthusiasts modifying their cars and professional workshops specialising in custom car audio installations.

Car speaker types and their applications. Which one to choose?

Car speakers, like HiFi speakers, are rated in terms of how much power they can handle. The basic models are: tweeter (suitable for high frequencies like cymbals), midrange (middle frequencies in the range of human voice, e.g., vocals), and woofer (designed to reproduce low-pitched audio frequencies. e.g., bass guitar). A broadband speaker will be adapted to the widest possible frequency range – but at the expense of overall quality. An intermediate solution is to use high-quality two-way car speakers, i.e., designed for low and medium or medium and high frequencies – for this purpose they incorporate two separate membranes.

The best effect is achieved by using high-quality crossovers (filter systems dividing the audio signal into low, medium, and high frequency ranges) and a set of 6 speakers (three for each stereo channel). Since the human ear cannot distinguish the direction of bass and woofers are big (their installation in the car can be troublesome), a channel combiner, an additional amplifier, and a single, dedicated woofer speaker are often used. A car sound system in this configuration (2+2+1) is the most preferred solution – as it allows for satisfactory results while minimising the space needed.

When buying car speakers, attention should be paid to at least two mechanical and electrical parameters. The first, of course, will be the size. Please note that the vast majority of cars (even If your vehicle does not have an audio system) have door speaker slots. Choosing a unit that is not suitable for a given car may involve the necessity to interfere with the structural elements of the vehicle, resulting in reduced rigidity and even compromising passenger safety. It is equally important to match car audio amplifiers to speakers. If your car is not equipped with an automotive external amplifier, this limitation will be imposed by the radio parameters.

Distances and speaker frames in car audio

"Aftermarket" loudspeakers (i.e., not dedicated to a specific car model) come in standard diameters and are fitted with standardised mounting holes. However, car manufacturers often use non-standard solutions, making it difficult to fit replacement audio components. This is where several suppliers offering assembly accessoriescome to the rescue. These include speaker frames and spacers. In both cases, the purpose is the same: these are adapters allowing a standard speaker to be fitted to a specific vehicle model. The car make and model, as well as the diameter of the speaker, are usually listed in the product specification. Usually, these parts are made of MDF or plastic, and all you need to assemble them is a spanner, screwdriver, and possibly a screwdriver. The latter will be required because not all frames have prefabricated mounting holes.

Rear car speakers. Small and heavy subwoofer enclosures

As already mentioned, one of the most effective ways to improve the capability of a sound system is to isolate the bass track and play it through a dedicated speaker, or subwoofer. There are three issues involved: firstly, such a speaker is relatively large in size (up to 30cm in diameter); secondly, it requires the use of a dedicated boxto bring out the low acoustic frequencies; thirdly, car manufacturers rarely include space for such a speaker in their designs (opting instead for specially designed units that fit into the doors or into the rear parcel shelf. If the car owner decides to add an additional woofer, they should consider using a special enclosure. These are wooden boxes covered with upholstery that perfectly fits the boot area. The TME catalogue offers not only universal enclosures, but also enclosures made for specific car models. In this case, the products are factory profiled to match the curves of the car. As a result, they ensure the maximum net volume, with only a slight effect on the load capacity of the luggage compartment.

Car audio accessories

Theacoustic accessories include foams, mats, and fabrics, which have three functions. First, they reduce buzz from the speaker cone. This eliminates unpleasant, "tinny" sound. Secondly, these materials reduce the interior and exterior noise of vehicles, which results in a more comfortable driving experience and improves your car audio experience. The third function is purely aesthetic and is mainly related to upholstery fabrics. These products are used for custom speaker systems (e.g. resonance boxes), as well as custom interior elements (additional compartments, slots, etc.). Here, the user can choose classic fabrics to match the car upholstery or eye-catching colour combinations. Fortunately, in this respect, we are limited only by our imagination...

Products: 893

Warehouse:

TME
All
Page 1
RAM-20.450/K | Speaker frame; 165mm; Audi,Seat,VW,Škoda; Audi A2 1999->; 2pcs.
Speaker frame; 165mm; Audi,Seat,VW,Škoda; Audi A2 1999->; 2pcs.
Manufacturer part number: RAM-20.450/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 3.67 USDGross price for quantities from 1 set - 3.67 USD
Net price for quantities from 3 set - 3.07 USDGross price for quantities from 3 set - 3.07 USD
Net price for quantities from 5 set - 2.60 USDGross price for quantities from 5 set - 2.60 USD
Net price for quantities from 10 set - 2.36 USDGross price for quantities from 10 set - 2.36 USD
2800 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.505/K | Speaker frame; 165mm; Audi,VW,Škoda; Audi Q3 (8U) 2011->2018
Speaker frame; 165mm; Audi,VW,Škoda; Audi Q3 (8U) 2011->2018
Manufacturer part number: RAM-20.505/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 3.67 USDGross price for quantities from 1 set - 3.67 USD
Net price for quantities from 3 set - 3.07 USDGross price for quantities from 3 set - 3.07 USD
Net price for quantities from 5 set - 2.60 USDGross price for quantities from 5 set - 2.60 USD
Net price for quantities from 10 set - 2.36 USDGross price for quantities from 10 set - 2.36 USD
590 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.435/K | Speaker frame; 165mm; Honda,Opel; Honda Jazz 2002->2008; 2pcs.
Speaker frame; 165mm; Honda,Opel; Honda Jazz 2002->2008; 2pcs.
Manufacturer part number: RAM-20.435/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 1.99 USDGross price for quantities from 1 set - 1.99 USD
Net price for quantities from 3 set - 1.67 USDGross price for quantities from 3 set - 1.67 USD
Net price for quantities from 5 set - 1.42 USDGross price for quantities from 5 set - 1.42 USD
Net price for quantities from 10 set - 1.28 USDGross price for quantities from 10 set - 1.28 USD
773 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
DMVW02 | Spacer ring; MDF; 165mm; VW; impregnated; 2pcs.
Spacer ring; MDF; 165mm; VW; impregnated; 2pcs.
Manufacturer part number: DMVW02
Manufacturer: BASSER
Net price for quantities from 1 set - 8.79 USDGross price for quantities from 1 set - 8.79 USD
Net price for quantities from 3 set - 7.81 USDGross price for quantities from 3 set - 7.81 USD
Net price for quantities from 5 set - 6.83 USDGross price for quantities from 5 set - 6.83 USD
Net price for quantities from 10 set - 6.35 USDGross price for quantities from 10 set - 6.35 USD
123 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.542/K | Speaker frame; 165mm; Audi,Seat,VW,Škoda; Audi A1 2010->,VW UP
Speaker frame; 165mm; Audi,Seat,VW,Škoda; Audi A1 2010->,VW UP
Manufacturer part number: RAM-20.542/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 4.86 USDGross price for quantities from 1 set - 4.86 USD
Net price for quantities from 3 set - 4.43 USDGross price for quantities from 3 set - 4.43 USD
Net price for quantities from 5 set - 3.81 USDGross price for quantities from 5 set - 3.81 USD
Net price for quantities from 10 set - 3.39 USDGross price for quantities from 10 set - 3.39 USD
356 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SC-M2 | Damping mat; aluminium foil,butyl rubber; 375x250x2mm
Damping mat; aluminium foil,butyl rubber; 375x250x2mm
Manufacturer part number: SC-M2
Manufacturer: SILENT COAT
Net price for quantities from 1 pcs - 3.40 USDGross price for quantities from 1 pcs - 3.40 USD
Net price for quantities from 5 pcs - 3.00 USDGross price for quantities from 5 pcs - 3.00 USD
Net price for quantities from 10 pcs - 2.72 USDGross price for quantities from 10 pcs - 2.72 USD
Net price for quantities from 20 pcs - 2.37 USDGross price for quantities from 20 pcs - 2.37 USD
221 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
CL-018165 | Car loudspeakers; two-way; 165mm; 120W; 65÷20000Hz; 4Ω; 90dB; 2pcs.
Car loudspeakers; two-way; 165mm; 120W; 65÷20000Hz; 4Ω; 90dB; 2pcs.
Manufacturer part number: CL-018165
Manufacturer: CL ITALIA
Net price for quantities from 1 set - 20.87 USDGross price for quantities from 1 set - 20.87 USD
Net price for quantities from 3 set - 18.55 USDGross price for quantities from 3 set - 18.55 USD
Net price for quantities from 5 set - 17.40 USDGross price for quantities from 5 set - 17.40 USD
Net price for quantities from 10 set - 16.24 USDGross price for quantities from 10 set - 16.24 USD
98 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
271230-07-0 | Speaker frame; 165mm; Citroën,Fiat,Opel,Peugeot; 2pcs.
Speaker frame; 165mm; Citroën,Fiat,Opel,Peugeot; 2pcs.
Manufacturer part number: 271230-07-0
Manufacturer: ACV
Net price for quantities from 1 set - 3.57 USDGross price for quantities from 1 set - 3.57 USD
Net price for quantities from 3 set - 3.20 USDGross price for quantities from 3 set - 3.20 USD
Net price for quantities from 5 set - 2.82 USDGross price for quantities from 5 set - 2.82 USD
Net price for quantities from 10 set - 2.63 USDGross price for quantities from 10 set - 2.63 USD
106 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
CL-018100 | Car loudspeakers; two-way; 100mm; 100W; 80÷20000Hz; 4Ω; 87dB; 2pcs.
Car loudspeakers; two-way; 100mm; 100W; 80÷20000Hz; 4Ω; 87dB; 2pcs.
Manufacturer part number: CL-018100
Manufacturer: CL ITALIA
Net price for quantities from 1 set - 15.04 USDGross price for quantities from 1 set - 15.04 USD
Net price for quantities from 3 set - 13.37 USDGross price for quantities from 3 set - 13.37 USD
Net price for quantities from 5 set - 12.54 USDGross price for quantities from 5 set - 12.54 USD
Net price for quantities from 10 set - 11.70 USDGross price for quantities from 10 set - 11.70 USD
71 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.497.2/K | Speaker frame; 165mm; Dacia Dokker 2013->2018; 2pcs.
Speaker frame; 165mm; Dacia Dokker 2013->2018; 2pcs.
Manufacturer part number: RAM-20.497.2/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 5.38 USDGross price for quantities from 1 set - 5.38 USD
Net price for quantities from 3 set - 4.55 USDGross price for quantities from 3 set - 4.55 USD
Net price for quantities from 5 set - 4.20 USDGross price for quantities from 5 set - 4.20 USD
Net price for quantities from 10 set - 3.69 USDGross price for quantities from 10 set - 3.69 USD
105 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
DMAUDI03 | Spacer ring; MDF; 165mm; Audi; impregnated; 2pcs.
Spacer ring; MDF; 165mm; Audi; impregnated; 2pcs.
Manufacturer part number: DMAUDI03
Manufacturer: BASSER
Net price for quantities from 1 set - 11.12 USDGross price for quantities from 1 set - 11.12 USD
Net price for quantities from 3 set - 9.88 USDGross price for quantities from 3 set - 9.88 USD
Net price for quantities from 5 set - 8.65 USDGross price for quantities from 5 set - 8.65 USD
Net price for quantities from 10 set - 8.03 USDGross price for quantities from 10 set - 8.03 USD
101 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
DMVW04 | Spacer ring; MDF; 165mm; VW; impregnated; 2pcs.
Spacer ring; MDF; 165mm; VW; impregnated; 2pcs.
Manufacturer part number: DMVW04
Manufacturer: BASSER
Net price for quantities from 1 set - 9.95 USDGross price for quantities from 1 set - 9.95 USD
Net price for quantities from 3 set - 8.85 USDGross price for quantities from 3 set - 8.85 USD
Net price for quantities from 5 set - 7.74 USDGross price for quantities from 5 set - 7.74 USD
Net price for quantities from 10 set - 7.19 USDGross price for quantities from 10 set - 7.19 USD
146 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
BOX0004-05 | Car loudspeaker enclosure; plastic; black; 100mm
Car loudspeaker enclosure; plastic; black; 100mm
Manufacturer part number: BOX0004-05
Manufacturer: PER.PIC.
Net price for quantities from 1 pcs - 9.96 USDGross price for quantities from 1 pcs - 9.96 USD
Net price for quantities from 3 pcs - 8.54 USDGross price for quantities from 3 pcs - 8.54 USD
Net price for quantities from 5 pcs - 7.59 USDGross price for quantities from 5 pcs - 7.59 USD
Net price for quantities from 10 pcs - 6.64 USDGross price for quantities from 10 pcs - 6.64 USD
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SU70009-05X2 | Speaker frame; 130mm; Renault; Renault Megane III 2008->; 2pcs.
Speaker frame; 130mm; Renault; Renault Megane III 2008->; 2pcs.
Manufacturer part number: SU70009-05X2
Manufacturer: PER.PIC.
Net price for quantities from 1 set - 6.86 USDGross price for quantities from 1 set - 6.86 USD
Net price for quantities from 3 set - 6.14 USDGross price for quantities from 3 set - 6.14 USD
Net price for quantities from 5 set - 5.42 USDGross price for quantities from 5 set - 5.42 USD
Net price for quantities from 10 set - 5.05 USDGross price for quantities from 10 set - 5.05 USD
83 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
271320-16-0 | Speaker frame; 165mm; Seat,VW,Škoda; Seat Arosa 1998->; 2pcs.
Speaker frame; 165mm; Seat,VW,Škoda; Seat Arosa 1998->; 2pcs.
Manufacturer part number: 271320-16-0
Manufacturer: ACV
Net price for quantities from 1 set - 4.90 USDGross price for quantities from 1 set - 4.90 USD
Net price for quantities from 3 set - 4.38 USDGross price for quantities from 3 set - 4.38 USD
Net price for quantities from 5 set - 3.87 USDGross price for quantities from 5 set - 3.87 USD
Net price for quantities from 10 set - 3.60 USDGross price for quantities from 10 set - 3.60 USD
51 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
DMVW06 | Spacer ring; MDF; 165mm; VW; impregnated; 2pcs.
Spacer ring; MDF; 165mm; VW; impregnated; 2pcs.
Manufacturer part number: DMVW06
Manufacturer: BASSER
Net price for quantities from 1 set - 9.95 USDGross price for quantities from 1 set - 9.95 USD
Net price for quantities from 3 set - 8.85 USDGross price for quantities from 3 set - 8.85 USD
Net price for quantities from 5 set - 7.74 USDGross price for quantities from 5 set - 7.74 USD
Net price for quantities from 10 set - 7.19 USDGross price for quantities from 10 set - 7.19 USD
143 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.460/K | Speaker frame; 6x9"; BMW; BMW 3 1991->1998; BMW 3 rear shelf
Speaker frame; 6x9"; BMW; BMW 3 1991->1998; BMW 3 rear shelf
Manufacturer part number: RAM-20.460/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 6.84 USDGross price for quantities from 1 set - 6.84 USD
Net price for quantities from 3 set - 6.16 USDGross price for quantities from 3 set - 6.16 USD
Net price for quantities from 5 set - 5.47 USDGross price for quantities from 5 set - 5.47 USD
Net price for quantities from 10 set - 4.79 USDGross price for quantities from 10 set - 4.79 USD
73 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
MDF-D.14 | Spacer ring; MDF; 165mm; Seat,VW,Škoda; impregnated,varnished
Spacer ring; MDF; 165mm; Seat,VW,Škoda; impregnated,varnished
Manufacturer part number: MDF-D.14
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 7.66 USDGross price for quantities from 1 set - 7.66 USD
Net price for quantities from 3 set - 6.81 USDGross price for quantities from 3 set - 6.81 USD
Net price for quantities from 5 set - 5.96 USDGross price for quantities from 5 set - 5.96 USD
Net price for quantities from 10 set - 5.53 USDGross price for quantities from 10 set - 5.53 USD
45 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.401/K | Speaker frame; 130mm; Audi; Audi A4 1994->2001; 2pcs.
Speaker frame; 130mm; Audi; Audi A4 1994->2001; 2pcs.
Manufacturer part number: RAM-20.401/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 1.43 USDGross price for quantities from 1 set - 1.43 USD
Net price for quantities from 3 set - 1.21 USDGross price for quantities from 3 set - 1.21 USD
Net price for quantities from 5 set - 1.01 USDGross price for quantities from 5 set - 1.01 USD
Net price for quantities from 10 set - 0.92 USDGross price for quantities from 10 set - 0.92 USD
530 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RAM-20.518.2/K | Speaker frame; 165mm; Citroën,Fiat,Opel,Peugeot; 2pcs.
Speaker frame; 165mm; Citroën,Fiat,Opel,Peugeot; 2pcs.
Manufacturer part number: RAM-20.518.2/K
Manufacturer: 4CARMEDIA
Net price for quantities from 1 set - 3.63 USDGross price for quantities from 1 set - 3.63 USD
Net price for quantities from 3 set - 3.06 USDGross price for quantities from 3 set - 3.06 USD
Net price for quantities from 5 set - 2.80 USDGross price for quantities from 5 set - 2.80 USD
Net price for quantities from 10 set - 2.52 USDGross price for quantities from 10 set - 2.52 USD
179 in TME stock
No. of complete sets (Multiplicity: 1)