+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The ampere (A) is the SI unit of electric current and one of the seven base units in the International System of Units. It defines the amount of electric charge passing through a point in a circuit per unit time—specifically, one coulomb per second. The unit is named after André-Marie Ampère, a 19th-century physicist and pioneer in the field of electromagnetism, whose work laid the foundation for the fundamental principles of electric current and its magnetic interactions.
As of the 2019 redefinition, the ampere is defined in terms of the elementary charge constant. According to this definition, one ampere corresponds to the flow of exactly 1⁄(1.602176634 × 10⁻¹⁹) electrons per second, which equals approximately 6.241 × 10¹⁸ elementary charges per second. This formulation ties the unit directly to fundamental physical constants, eliminating reliance on the macroscopic properties of measuring instruments and ensuring consistency and precision.
In practice, the ampere quantifies the intensity of current flowing through an electrical circuit. The current level directly affects the design, operation, and safety of electrical components such as transformers, conductors, fuses, and power supplies. It is also a key factor in electrical protection systems, particularly in safeguarding against thermal overloads and electric shock hazards. The ampere interacts with other units such as the volt and the ohm, forming relationships described by Ohm’s law, which links voltage, current, and resistance.
Current measurement is typically performed using an ammeter, which may be a standalone instrument or integrated into a multimeter. In both direct current (DC) and alternating current (AC) applications, knowing the value in amperes is essential for managing energy flow and preventing overloads or damage to electrical equipment.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.