+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Ohm (Ω) is the SI unit of electrical resistance, used to express the ability of a circuit element to limit the flow of electric current under an applied voltage. A resistance of one ohm occurs when a current of one ampere flows through a conductor with an applied voltage of one volt. According to Ohm’s law, resistance is defined as the ratio of voltage to current and plays a fundamental role in the analysis of electrical circuits.
The unit is named after the German physicist Georg Simon Ohm, who in the 19th century formulated empirical laws describing electrical conductivity. In engineering practice, resistance is expressed not only in ohms but also in its multiples and submultiples, such as kiloohm (kΩ), megaohm (MΩ), or milliohm (mΩ), depending on the characteristics of the system being analyzed and the level of resistance involved.
Electrical resistance is a scalar quantity and depends on the properties of the material, its geometry, and temperature. For metallic conductors, resistance increases with temperature, while in semiconductors and nonlinear materials this relationship can be more complex. Resistance affects power loss in the form of heat, which must be considered when designing electronic and power systems.
The ohm also plays an important role in the measurement, diagnostics, and regulation of operating parameters in electronic devices. In practical applications such as consumer electronics, power systems, or industrial automation, resistance measurement allows for the assessment of component condition, circuit continuity testing, and analysis of conductive and insulating material properties. Due to its universality and precise definition, the ohm remains one of the fundamental physical units used in electrical engineering and electronics.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.