+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
AWG (American Wire Gauge) is a standard for designating the diameter of electrical conductors, primarily used in the United States and Canada. It is based on a numerical scale in which a higher number corresponds to a thinner wire, while a lower number indicates a thicker one. The scale, developed in the 19th century for copper wires, follows a logarithmic progression, meaning the changes in gauge numbers are not linear in relation to the actual diameter or cross-sectional area.
The AWG standard defines not only wire diameter, but also the corresponding cross-sectional area, specific electrical resistance, wire length per unit mass, and typical current-carrying capacities. This enables precise specification of wire properties for the design of electrical and electronic systems. AWG is used in residential and industrial wiring as well as in the construction of electronic devices, where selecting the appropriate wire gauge affects both safety and system performance.
Conformance of a wire to a given AWG size directly impacts operational parameters such as voltage drop, heating, and overload tolerance. The system is widely referenced in technical documentation, catalog specifications, and wire labeling in both commercial and manufacturing contexts. Although square millimeter measurements are more common in Europe, AWG remains an important reference across many industries—especially where cooperation with the North American market is involved.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.