+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Zener diode - definition

A Zener diode is a specialized type of semiconductor diode designed to operate in reverse bias within a defined breakdown voltage range, which is precisely set during the manufacturing process. Unlike a standard diode, which blocks current flow in reverse bias until breakdown damage occurs, a Zener diode maintains a stable voltage across its terminals even under significant changes in current once the breakdown threshold is reached. This phenomenon, known as the Zener effect, is primarily used for voltage regulation in electronic circuits.

The operation of a Zener diode is based on controlled breakdown in the p–n junction, which may occur via tunneling (Zener breakdown) or avalanche multiplication, depending on the voltage level. When the reverse voltage reaches the specified Zener voltage, the diode conducts sharply while holding the voltage nearly constant across the junction. This characteristic makes the Zener diode an effective precision voltage regulator, independent of variations in load or supply conditions.

In practical applications, Zener diodes are commonly used for overvoltage protection, as reference elements in linear voltage regulators, and as voltage limiters in signal paths. The selection of a suitable model depends on the breakdown voltage, permissible power dissipation, and temperature stability. The Zener diode is an essential component in the design of reliable and voltage-resilient electronic systems, particularly where accurate control of power supply conditions is required.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO