+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Interface - definition

Interface is a technical term referring to a set of rules, mechanisms, and structures that enable communication between different components of a system—both at the hardware and software levels. It may involve a physical connection between devices or a logical layer for information exchange between programs, modules, or between a user and a machine. The purpose of an interface is to ensure operational compatibility and provide an unambiguous method for transmitting data, commands, or signals between cooperating components.

In a hardware context, an interface typically denotes a connector, transmission protocol, and a set of parameters that define how electronic devices interact. Examples include USB, HDMI, I²C, SPI, or PCI Express—each of these technologies defines both the physical connection and the method for encoding and synchronizing data. In computer systems, hardware interfaces determine component compatibility and influence the performance of data transmission between them.

In the field of programming, an interface refers to the point of interaction between different software components, such as libraries, modules, or operating systems. It specifies the set of accessible functions, data structures, parameters, and return types that must be adhered to by developers. Programming interfaces (APIs) facilitate modular, independent software development while maintaining encapsulation principles.

In human–computer interaction, the interface takes the form of graphical, textual, or touch-based elements and defines how the user communicates with the system. Interface design in this area involves ergonomics, accessibility, and usability. Regardless of the application domain, the interface is a fundamental element of integration and cooperation in complex technical systems, enabling their effective, secure, and flexible utilization.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO