+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Laminate - definition

Laminate is a multilayer composite material created by permanently bonding at least two different layers with distinct mechanical, chemical, or electrical properties. The aim of such a structure is to obtain a material with desired functional characteristics that cannot be achieved using a single raw component. Laminates are widely used in engineering, electronics, construction, and industry, where durability, strength, insulation, or resistance to environmental conditions are required.

In electronics, laminate most commonly refers to the base material used for manufacturing printed circuit boards (PCBs). It consists of a dielectric layer—typically made from phenolic paper or fiberglass fabric impregnated with epoxy resin—and an outer copper layer, which forms the conductive traces. These types of laminates must exhibit appropriate dielectric properties, thermal stability, low moisture absorption, and chemical resistance to ensure the reliable operation of electronic circuits.

The laminate manufacturing process involves pressing and curing material layers under controlled temperature and pressure conditions. Depending on the application, laminates may be reinforced with structural fibers such as glass, carbon, or aramid, while synthetic resins with carefully selected physicochemical properties serve as the binding agent. The composition and structure of the laminate are tailored to achieve the desired stiffness, flexibility, thermal conductivity, or electrical insulation.

Depending on the technical context, the term laminate may also refer to finishing materials, protective layers, or composites used in aerospace, automotive, or energy sectors. A critical aspect is the proper bonding and durability of the layers, which determine the quality and reliability of the final product in demanding operating environments.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO