+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

How do the basic components of integrated circuits work?

Date of publication: 21-02-2025 Update date: 07-11-2026 🕒 5 min read

Ever wondered what makes electronic devices such as smartphones, laptops or even modern refrigerators work so smoothly? At the heart of most of these devices are integrated circuits - small, black "chips" that hide all the magic of electronics.

Although they may seem complicated at first glance, their operation is truly fascinating. Learn what integrated circuits are and what they consist of - from the basics.

What is an integrated circuit? Types of integrated circuits

Integrated Circuit (IC - Integrated Circuit) is a tiny wafer made of silicon, enclosed in a plastic or ceramic housing. It contains hundreds, thousands or even millions of microscopic components, such as transistors, resistors and capacitors.

All these components work together to form more complex circuits that perform tasks related to, for example:

  • data processing;
  • controlling devices;
  • storing information.

There are several types of integrated circuits, depending on their application:

  1. Digital integrated circuits - used in computers, smartphones and other digital devices. They process information in the form of zeros and ones.
  2. Analog integrated circuits - amplifiers, signal converters that convert analog signals to digital and vice versa.
  3. Mixed ICs - combine digital and analog functions, such as in audio devices.

What exactly do they consist of?

Basic components of integrated circuits

In integrated circuits you will find many different components that together form functional circuits. The most important of these are transistors, resistors, capacitors, diodes and inductors.

Transistors

A transistor is a semiconductor electronic component used to control the flow of current. It can function as:

  1. Switch - controls the flow of current in logic circuits.
  2. Amplifier - amplifies electrical signals in analog circuits.

Bipolar transistors are used in analog circuits and amplifiers and operate by the flow of charge carriers (electrons and holes). They are controlled by the current flowing to the base. There are NPN type transistors (current flows from emitter to collector) and PNP type transistors (current flows in reverse).

They consist of three semiconductor layers:

  • Emitter (E): introduces charge carriers.
  • Base (B): thin layer that controls the flow of carriers.
  • Collector (C): receives the charge carriers.

Field-effect transistors (unipolar) control the flow of current by means of an electric field, not the base current. They have three leads:

  • Source (S): introduces charge carriers.
  • Gate (G): controls the flow of carriers by means of voltage.
  • Drain (D): takes away the charge carriers.

We distinguish unipolar transistors of the MOSFET type, which is the most popular element of this type. It is characterized by high switching speed and low power consumption. Another type is IGBTs (Insulated-Gate Bipolar Transistor), which are a hybrid of a bipolar transistor and a MOSFET. They feature high efficiency in switching currents at high voltages. They are used in power systems such as inverters, electric motors and power systems. SiC transistors, made with silicon carbide technology, should also be mentioned. They feature better performance at high temperatures and voltages. They are used in power electronics, automotive and high-power systems.

Resistors

Resistors are components that limit current flow to protect other components and regulate voltage. They feature a constant resistance value that reduces the current flowing through the circuit.

How does a resistor work? The flow of current causes a voltage drop in the component. It's like the constriction of a pipe - the volume of flowing water (current) decreases when it encounters resistance.

Capacitors

Capacitors store and release electrical energy. They act like small batteries, but their role in circuits is much more dynamic. They consist of two conductive plates separated by a dielectric (insulator).

These elements, depending on the voltage on the plates, rapidly accumulate and release charge. This makes them ideal for voltage stabilization and signal filtering (noise removal).

Diodes

Semiconductor diodes are basic electronic components that allow electric current to flow in one direction and block it in the opposite direction. They are made of semiconductor materials, such as silicon (Si) or germanium (Ge), which have specific properties that allow them to control the flow of current.

Semiconductor diodes work by combining two types of semiconductor materials: an N-type (with an excess of electrons) and a P-type (with an excess of "holes," or places where electrons are missing). This combination forms a PN junction, which has unique properties:

  • Current flow in one direction: When the diode is polarized in the straight direction (anode connected to the positive pole, cathode to the negative pole), electrons from the N-type region move to the P-type region, allowing current to flow.
  • Stopping current in the reverse direction: When a diode is reverse-polarized (anode connected to the negative pole, cathode to the positive pole), the PN junction blocks current flow. In this case, the current practically does not flow, unless there is a voltage at which a breakthrough occurs.

Inductors

Inductors are components that store energy in the form of a magnetic field. They are coils of wire - they store energy when current flows through them. Then a field is created around them, which disappears when the current stops flowing, and the stored energy is released.

What determines that the listed components are crucial to the operation of devices - from the simplest to advanced computers? Together they form functional circuits in which each unit has a function:

  • transistors are the "brain" of circuits, managing the flow of information;
  • resistors and capacitors regulate and stabilize current flow;
  • diodes protect circuits from errors;
  • inductors store energy.

How is an integrated circuit made?

The process of manufacturing an integrated circuit is extremely precise and complex. It uses special photolithography techniques to create microscopic structures on the surface of a silicon wafer (known as a wafer). It proceeds in 4 steps.

Step 1: Preparation of the silicon wafer - the silicon wafer is cleaned and covered with a thin layer of semiconductor material.

Step 2: Photolithography - with the help of UV light and special masks, patterns are applied that will form the paths and circuit elements.

Step 3: Doping - dopants are introduced into the silicon to change its conductive properties.

Step 4: Assembly - finished wafers are cut into individual chips, which are then encapsulated.

IC production takes place in special clean rooms (clean rooms), where the level of contaminants, such as dust, pollen or even microscopic particles, is strictly controlled. To maintain cleanliness, workers wear special coveralls, masks, gloves and shoe protectors - even the slightest contamination could damage the delicate structures on the silicon wafer.

In the production process, it is also extremely important to maintain stable temperature and humidity conditions, as even slight fluctuations can affect the quality of semiconductors. Processes such as photolithography, etching and doping are carried out under vacuum conditions or in the presence of special gases, which allows the precise formation of microscopic structures.

These rigorous standards enable integrated circuits to be not only miniature, but also extremely reliable, which is crucial in modern electronic devices.

Why are integrated circuits so important?

With the introduction of integrated circuits, it has become possible:

  • reducing the size of devices - computers used to take up entire rooms, today they fit in a pocket;
  • lower production costs - thanks to miniaturization, electronics are cheaper and more accessible;
  • increased efficiency - integrated circuits allow faster processing of data, which is crucial in modern technologies.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO