+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Annihilation - definition

Annihilation is a physical process, in which a particle and its antiparticle meet and annihilate each other, leading to the transformation of their rest mass into energy - usually in the form of electromagnetic radiation. This phenomenon occurs in accordance with the principle of conservation of energy and momentum, as well as other fundamental laws of physics, such as the conservation of electric charge, baryon or lepton number.

The best known example of annihilation is the interaction of an of the electron with positron, or its antiparticle. As a result of this reaction both particles disappear, and two or more photons gamma photons, whose total energy corresponds to the combined mass and kinetic energy of the annihilating particles. In laboratory conditions and in medical imaging technologies, such as positron emission tomography (PET), electron annihilation-positron plays a key role as a source of precise information about the distribution of the radioactive tracer in the body.

Annihilation can also occur between other particle-antiparticle pairs, such as proton-antiproton or neutron-antineutron, but in these cases the accompanying processes are more complex and often lead to the formation of mesons, which in turn decay into other particles. The phenomenon of annihilation has also a cosmological significance - it is an inseparable element of the Big Bang models and of the evolution of the early Universe, in which mutual annihilations of particles and antiparticles influenced the formation of present-day matter.

The mechanism of annihilation is described by particle physics and quantum field theory, in particular quantum electrodynamics. Annihilation observations and experiments are crucial for the study of antimatter, fundamental symmetries and for the development of accurate particle detection methods.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO