+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Areometer - definition of

Areometer is a measuring instrument used to determine the relative density of liquids or liquids containing dissolved solids, using the buoyancy principle described by Archimedes. It usually consists of a glass tube with an expanded lower part, weighted so as, so that it remains vertical when immersed in a liquid. A scale calibrated in units of relative density is attached to the stem of the hydrometer, specific gravity, percentage of dissolved substance (e.g. alcohol, sugar) or the Baume, Brix, API or Plato - depending on the industrial application.

The principle of the areometer is based on measuring the depth of its immersion in the liquid under test: the higher the density of the, the smaller the immersion. The preconditions for correct measurement are an isothermal measuring environment and the absence of mechanical impurities and gas bubbles, which may distort the result. Precise readings are obtained at the liquid meniscus level, usually read at the level of contact between the liquid and the tube, assuming that the body material is wetted.

Areometers are commonly used in the chemical industry, food industry (e.g. brewing, oenology), pharmaceutical and petrochemical industries. Today, there are also digital and electronic versions, which allow automatic reading and recording of results with temperature correction and calibration for different reference liquids. In technical and industrial laboratories, areometry is a simple, a simple yet highly reproducible measurement method, without a complex analytical infrastructure.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO