+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Bit error rate (BER) - definition

Bit Error Rate (BER, Bit Error Rate) is a coefficient that determines the quality of data transmission in digital systems. It expresses the ratio of the number of erroneously transmitted bits to the total number of bits received in a given time interval or within a given transmission sample. BER is a dimensionless value, most often represented as a decimal fraction or exponential number.

This parameter is crucial for assessing the reliability of telecommunications systems, Computer Networks, satellite transmission systems or radio equipment. A low BER value indicates high transmission quality and low interference, while higher values may indicate the presence of signal propagation problems, electromagnetic interference, hardware imperfections or errors in synchronisation.

BER is usually measured statistically by analysing reference data of known structure transmitted by the channel under test. The receiver compares it with the original by counting the number of discrepancies. In transmission systems, BER can be reduced through the use of methods correction coding, modulation of the noise-tolerant signal or adaptive techniques that adjust the transmission parameters to the channel conditions.

Accurate BER control is important not only for data integrity, but also for bandwidth efficiency and transmission delay. In applications requiring high reliability, such as aerospace, medical or space, the acceptable BER value can sometimes be extremely low, while in less critical applications it can be tolerated at a higher level, as long as the functionality of the system is not significantly affected.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO