+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Densimeter - definition

A Densimeter is a measuring instrument used to determine the density or specific gravity of liquids and sometimes semi-solids. Its operation is based on Archimedes' buoyancy principle, according to which the buoyancy force acting on an immersed body is equal to the weight of the fluid it displaces. In practice, the densimeter takes the form of a glass or plastic cylinder with a ballast at the bottom and a measuring scale at the top for direct reading of the density value.

During measurement, the densimeter is immersed in the liquid under test and fixed in an equilibrium position, the depth of immersion depending on the density of the liquid. The value is read at the level of the meniscus of the liquid on a calibrated scale. The scale of the densimeter can be graduated in different units: g/cm³, kg/m³, degrees Baumé, API, Brix or Plato - depending on the specific industry application.

Densimeters are widely used in the food industry (e.g. control of sugars in beverages), chemical, pharmaceutical and petrochemical industries, as well as in analytical laboratories. The precision of the measurement depends on the temperature of the liquid, which is why modern densimeters can be equipped with temperature compensation or work with reference thermometers.

Modern versions of densimeters, including oscillating digital densimeters, offer automatic measurement based on a change in the frequency of oscillation of the measuring tube filled with the sample under investigation. Such devices are characterised by high sensitivity, short measurement times and the possibility of recording and transmitting data to quality management systems or laboratory analysis.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO