+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
DSSS (Direct Sequence Spread Spectrum) is a technique for modulation and signal transmission in wireless communication systems, which involves spreading the spectrum of the usable signal using a pseudo-random sequence at a much higher frequency than the original information signal. As a result of this process, the signal power is spread over a wider frequency band, increasing the transmission's resistance to interference, eavesdropping and interference.
A key element of DSSS is the spreading code, also known as the spreading sequence or PN (Pseudo-Noise) code. Each bit of data is multiplied by a sequence of higher frequency bits, creating what are known as chips. This process causes the signal to occupy a much wider bandwidth than that required to transmit the information, making it difficult for third parties to detect and interfere with it. On the receiving side, the signal is reconstructed by correlating with the same PN sequence, restoring the original data.
Thanks to its scattering properties, DSSS is immune to narrowband interference and allows multiple channels to coexist in the same frequency range. The technique is used, among others, in GPS systems, mobile telephony and wireless communication standards such as IEEE 802.11b. For military and specialised applications, DSSS offers an additional layer of security due to the difficulty of intercepting and analysing the signal without knowledge of the scatter code.
Compared to other spread spectrum techniques, DSSS has a relatively simple implementation and high transmission quality in noisy environments. The performance of DSSS depends on the parameters of the PN code, synchronisation of the receiver and the quality of the transmission path.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.